IMX6UL如何降低SIM模块的频率

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL如何降低SIM模块的频率

2,110 Views
jasonshao
Contributor II

我现在使用的SIM模块的设备节点是这样的:pastedImage_1.png

这样SIM模块获取到的时钟频率是240MHz,使用最大的分频参数255后的频率是941KHz,我在读取synchronous 卡的时候,需要频率在 300KHz以内才可以,所以怎么才可以降低这个频率,我尝试调整了assigned-clock-rates的数值,但是,无论我将这个地方设置为多少,在驱动里通过 clk_get_rate 得到的频率数都是 240MHz,看上去调整这里并不起作用,谁能帮忙看下该怎么调整这个频率?

Labels (3)
0 Kudos
Reply
2 Replies

2,001 Views
jasonshao
Contributor II

Hi Joan,

        谢谢你的回复,但是我还是有些不太明白,你能说下具体怎么修改吗?谢谢!

0 Kudos
Reply

2,001 Views
joanxie
NXP TechSupport
NXP TechSupport

for example, sim_podf is Divider for SIM clock divider, maybe you can change this to change the clock, more detailed information, you need refer to the Reference Manual, you can try to change this then see what happens

0 Kudos
Reply