IMX6SoloX consumption calculation file for use conditions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6SoloX consumption calculation file for use conditions

ソリューションへジャンプ
1,161件の閲覧回数
takashitakahash
Contributor III

Hi, Community.

Our customer has question of about IMX6SoloX  consumption calculation file for use conditions.

Would you please give us  like a presentation of current consumption calculation file for use conditions or use case.

IMX6SXAEC Rev. 1, 9/2015 Datasheet  of p31 description of

Primary Interface (IO) Supplies are all "-" (bar),that represents what is mean?

ラベル(3)
0 件の賞賛
返信
1 解決策
972件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

"Supplies are all "-" (bar)"  means that there are no special conditions.

Regarding current consumption calculation one can use formula

i.MX6DQ Datasheet (rev.4, 7/2015) given at footnote 5

Table 8. Maximum Supply Currents

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

5 General equation for estimated, maximum power consumption of an IO power supply:

Imax = N x C x V x (0.5 x F)

Where:

N—Number of IO pins supplied by the power line

C—Equivalent external capacitive load

V—IO voltage

(0.5 xF)—Data change rate. Up to 0.5 of the clock rate (F)

In this equation, Imax is in Amps, C in Farads, V in Volts, and F in Hertz.

May be useful AN5050 i.MX 6SoloX Power Consumption Measurement

cache.freescale.com/files/32bit/doc/app_note/AN5050.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
973件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

"Supplies are all "-" (bar)"  means that there are no special conditions.

Regarding current consumption calculation one can use formula

i.MX6DQ Datasheet (rev.4, 7/2015) given at footnote 5

Table 8. Maximum Supply Currents

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

5 General equation for estimated, maximum power consumption of an IO power supply:

Imax = N x C x V x (0.5 x F)

Where:

N—Number of IO pins supplied by the power line

C—Equivalent external capacitive load

V—IO voltage

(0.5 xF)—Data change rate. Up to 0.5 of the clock rate (F)

In this equation, Imax is in Amps, C in Farads, V in Volts, and F in Hertz.

May be useful AN5050 i.MX 6SoloX Power Consumption Measurement

cache.freescale.com/files/32bit/doc/app_note/AN5050.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信