IMX6SX SDB PCIe + ATH9K(AR9280) performance problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SX SDB PCIe + ATH9K(AR9280) performance problem

1,298 Views
yulsangkim
Contributor I

Hi

I am testing the pcie + ar9280 (wifi) performance on the imx6sx board. Transmission performance is below 10Mbps. Therefore, when debugging, ath_isr () printk message of the Linux ath9k device driver is output, the transmission performance is more than 50Mbps.

1. Is the PCIe or ATH9K driver a problem?
2. What is the solution?

I need help.

Labels (2)
0 Kudos
Reply
1 Reply

1,135 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yulsang

one can look for wifi modules which are optimized and supported in nxp official linux bsps:

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Linux documentation

i.MX Software|NXP 

i.MX6Q PCIe throughput figures can be found on

https://community.nxp.com/docs/DOC-95014 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply