IMX6SX - EIM specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SX - EIM specification

Jump to solution
1,742 Views
JHY
Contributor IV

eim.jpg

IMX6SXRM.pdf say that each CS can use 128MB like above.

So totally 512MBytes memory can be used. Is it right?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,630 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

Total address space size is 128 MByte.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,631 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

Total address space size is 128 MByte.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------