IMX6SX BT1120

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SX BT1120

Jump to solution
2,034 Views
moowonlee
Contributor II

hi 

is it possible for imx6sx to support  BT1120? 

0 Kudos
Reply
1 Solution
1,861 Views
igorpadykov
NXP Employee
NXP Employee

Hi moowon

i.MX6SX CSI and eLCDIF modules support BT656 but not BT1120,

for CSI one can try to use bayer input format.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,862 Views
igorpadykov
NXP Employee
NXP Employee

Hi moowon

i.MX6SX CSI and eLCDIF modules support BT656 but not BT1120,

for CSI one can try to use bayer input format.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------