IMX6SOLO interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6SOLO interrupt

1,012 次查看
lihao1993
Contributor I

I want to know which pins of IMX6SOLO can be used as an interrupt pin, and which tube feet can wake up IMX6SOLO from low-power mode

标签 (1)
1 回复

938 次查看
art
NXP Employee
NXP Employee

All of the i.MX6Solo pins that have the GPIO function multiplexed can be configured to operate as the GPIO interrupt source, and any of these interrupts can wake the processor up from low-power mode.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------