IMX6SLEVK debug uart problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SLEVK debug uart problems

Jump to solution
1,802 Views
egorrumjantsev
Contributor III

Hi.

I received IMX6SLEVK and try to bring up u-boot working for it. I compiled U-Boot from Denx site for this board.

I see that U-Boot send debug output to debug UART, via serial console on my Linux PC but i can't sent anything back. TX line doesn't work....even i tri to see with oscilloscope - no data from FT232RQ TX pin.

Maybe the problem in ftdi_sio driver in mt PC? I'm using kernel 2.6.39, so i took driver from 3.4 branch and put it in my current kernel. The reason the same - no TX data.

I checked Android's images from cards that shipped with board, but had same situation.

Why that can happen?

WBR,

Labels (1)
0 Kudos
Reply
1 Solution
1,691 Views
fabio_estevam
NXP Employee
NXP Employee

Double check your terminal settings, such as no flow control.

Regards,

Fabio Estevam

View solution in original post

0 Kudos
Reply
2 Replies
1,692 Views
fabio_estevam
NXP Employee
NXP Employee

Double check your terminal settings, such as no flow control.

Regards,

Fabio Estevam

0 Kudos
Reply
1,691 Views
egorrumjantsev
Contributor III

Yes, seems the problem was in flow control.

It is very strange....cu doesn't have flow control options and i use it whithout such problems with other devices.

In fact i tried minicom and it worked better.

Thank you!

0 Kudos
Reply