IMX6S + LPDDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6S + LPDDR2

3,026 Views
zhanghaijian
Contributor II

Dear,everyone,

    I designed a board with imx6s + lpddr2。The uboot can booting now,but the kernel is hanging at "Uncompressing Linux... done, booting the kernel".The uboot output log , DCD config table and Schematic ,pls refer to the attachment. and give me some advise!.Best Regards,

Original Attachment has been moved to: uboot-log.txt.zip

Original Attachment has been moved to: imximage_mx6dl.cfg.zip

Labels (1)
0 Kudos
Reply
3 Replies

2,714 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

please run ddr test and update *.cfg file with new calibration settings found from test

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,714 Views
zhanghaijian
Contributor II

Hello igor,

I tested the memory with the “i.MX6/7 DDR Stress Test Tool V2.70”,The output log is:
============================================
        DDR Stress Test (2.6.0) 
        Build: Aug  1 2017, 17:33:18
        NXP Semiconductors.
============================================
============================================
        Chip ID
CHIP ID = i.MX6 Solo/DualLite (0x61)
Internal Revision = TO1.2
============================================
============================================
        Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00001040
SRC_SBMR2(0x020d801c) = 0x22000001
============================================
ARM Clock set to 1GHz
============================================
        DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is LPDDR2 in 1-channel mode.
Data width: 32, bank num: 8
Row size: 14, col size: 10
Both chip select CSD0 and CSD1 are used  
Density per chip select: 512MB 
Density per channel: 1024MB 
============================================
Current Temperature: 59
============================================
DDR Freq: 396 MHz 
Note: Array result[] holds the DRAM test result of each byte.  
      0: test pass.  1: test fail  
      4 bits respresent the result of 1 byte.    
      result 0001:byte 0 fail. 
      result 0011:byte 0, 1 fail. 
Starting Read calibration...
ABS_OFFSET=0x00000000 result[00]=0x1111
ABS_OFFSET=0x04040404 result[01]=0x1111
ABS_OFFSET=0x08080808 result[02]=0x1111
ABS_OFFSET=0x0C0C0C0C result[03]=0x1111
ABS_OFFSET=0x10101010 result[04]=0x1111
ABS_OFFSET=0x14141414 result[05]=0x1111
ABS_OFFSET=0x18181818 result[06]=0x1111
ABS_OFFSET=0x1C1C1C1C result[07]=0x1111
ABS_OFFSET=0x20202020 result[08]=0x1111
ABS_OFFSET=0x24242424 result[09]=0x1111
ABS_OFFSET=0x28282828 result[0A]=0x1111
ABS_OFFSET=0x2C2C2C2C result[0B]=0x1111
ABS_OFFSET=0x30303030 result[0C]=0x1111
ABS_OFFSET=0x34343434 result[0D]=0x1111
ABS_OFFSET=0x38383838 result[0E]=0x1111
ABS_OFFSET=0x3C3C3C3C result[0F]=0x1111
ABS_OFFSET=0x40404040 result[10]=0x1111
ABS_OFFSET=0x44444444 result[11]=0x1111
ABS_OFFSET=0x48484848 result[12]=0x1111
ABS_OFFSET=0x4C4C4C4C result[13]=0x1111
ABS_OFFSET=0x50505050 result[14]=0x1111
ABS_OFFSET=0x54545454 result[15]=0x1111
ABS_OFFSET=0x58585858 result[16]=0x1111
ABS_OFFSET=0x5C5C5C5C result[17]=0x1111
ABS_OFFSET=0x60606060 result[18]=0x1111
ABS_OFFSET=0x64646464 result[19]=0x1111
ABS_OFFSET=0x68686868 result[1A]=0x1111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111
ABS_OFFSET=0x70707070 result[1C]=0x1111
ABS_OFFSET=0x74747474 result[1D]=0x1111
ABS_OFFSET=0x78787878 result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111
ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values. 
Error: failed during ddr calibration
Best Regards.
0 Kudos
Reply

2,714 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

for error descriptions please check

Freescale i.MX6 DRAM Port Application Guide-DDR3 

and FAQ section on:

i.MX6/7 DDR Stress Test Tool V2.70 

Best regards
igor

0 Kudos
Reply