IMX6QP analog video and memory bandwidth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6QP analog video and memory bandwidth

1,092件の閲覧回数
vaudoitlaurent
Contributor IV

Hi,
we are using an isl79987 chip for capturing up to 4 analog camera.

I've applied the patch from nxp wich allow 4 channel capturing and displaying on a hdmi screen on a 4.19 kernel (using nxp bsp)
Test are done using the nxp test application mxc_v4l2_tvin.out
below the command launch:

./mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -m 1 -g2d &
./mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -m 1 -g2d &
./mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -m 1 -g2d &
./mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -m 1 -g2d &


Everything works now, and i'm trying to understand the impact on cpu and ram.
For this i use htop (for cpu side) and mmdc tools for memory side.

I see that CPU load is not so much, which can be explained by the fact that most of the work is done by the IPU.

The question is more on the mmdc result:

0 channel:
ipu1: utilization: 27%
overall bus load: 10%
ipu2: utilization: 0%
overall bus load: 0%

1 channel capture and display:
ipu1: utilization: 42%
overall bus load: 15%
ipu2: utilization: 0%
overall bus load: 0%

2 channel capture and display:
ipu1: utilization: 35%
overall bus load: 19%
ipu2: utilization: 4%
overall bus load: 23%

3 channel capture and display:
ipu1: utilization: 28%
overall bus load: 24%
ipu2: utilization: 4%
overall bus load: 23%

4 channel capture and display:
ipu1: utilization: 26%
overall bus load: 27%
ipu2: utilization: 5%
overall bus load: 27%


I don't really understand why with only 2 channel, IPU2 load the ram bus.
And after, if we add channel3 and 4, IPU2 overall bus load seems to follow ipu1 overall bus load.

Moreover, does this mean that with 4 channel, memory bus load is 27% or 54%?

Would you have some explaination, or could you indicate where i can find some informations on how it is working?

Thans in advance.

Regards
Laurent

0 件の賞賛
返信
3 返答(返信)

1,039件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Laurent

>I don't really understand why with only 2 channel, IPU2 load the ram bus.

one can look at Figure 19-1. CSI2IPU gasket connectivity, Figure 45-1. NIC-301 Bus System

i.MX 6Dual/6Quad Applications Processor Reference Manual

NIC301 details in AN4947:

https://www.nxp.com/docs/en/application-note/AN4947.pdf 

Utilization, bus load are well described on

IMX6 Memory Bandwidth Usage | iMX6 Board Memory 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,039件の閲覧回数
vaudoitlaurent
Contributor IV

Hi Igor,

thanks for the answer.

Regarding CSI2IPU gasket, i had seen this before, but as in the device tree we set 

mipi-csi2-channel0 with : ipu_id=0, csi_id=0,v_channel = 0

mipi-csi2-channel1 with : ipu_id=0, csi_id=1,v_channel = 1

mipi-csi2-channel2 with : ipu_id=1, csi_id=0,v_channel = 2

mipi-csi2-channel3 with : ipu_id=1, csi_id=1,v_channel = 3

and mxc-v4l2-capture like this:

v4l2_cap_0: ipu_id=0 csi_id = 0

v4l2_cap_0: ipu_id=0 csi_id = 1

v4l2_cap_1: ipu_id=0 csi_id = 0

v4l2_cap_1: ipu_id=0 csi_id = 0

i was thinking that for capture on /dev/video0 and /dev/video1, only ipu 0 would be used.

For the NIC, i'm not sure this apply to our setup as we are on a imx6 platform.

Regards

Laurent 

0 件の賞賛
返信

1,039件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Laurent 

NIC is present on all imx6 platforms.

Best regards
igor

0 件の賞賛
返信