IMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q

3,433 Views
vittoria98
Contributor I

Hello, in trying to test a board usign XJTAG link2. The board has an IMX6Q. I've checked the pin mapping and reset sequence but when I try to check the chain, it shows the same error: 

No valid data returned from the JTAG chain.
Perhaps the pin map is incorrect, or the board is not powered.

 

Check Chain failed

 

How can I fix this error?

0 Kudos
Reply
7 Replies

3,423 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @vittoria98,

I hope you are doing well.

One can refer to Example 3: No Valid Data Returned from the below link to know the possible causes of the error:

https://www.xjtag.com/support/application-notes/jtag-chain-debugging/

In addition to the above, could you please also check what is the status of the JTAG reset pin?

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

3,420 Views
vittoria98
Contributor I

Hi @riteshmpatel thank you for your answer, 

I've already checked the status of the JTAG reset pin and it should be alright, and also I've set the reset sequence. 

Do you have any other suggestion?

0 Kudos
Reply

3,415 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @vittoria98,

You may refer to the below link which describes the different errors faced by JTAG.

https://www.xjtag.com/support/application-notes/jtag-chain-debugging/

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

3,406 Views
vittoria98
Contributor I

Hi @riteshmpatel, I still have the same error... 

How can I be sure that the test reset sequence I'm using is the right one? 

Thank you, 

Vittoria

0 Kudos
Reply

3,390 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @vittoria98,

Apologies for the delay in response.

1. For the JTAG Connection/Test sequence

Please try the JTAG Connection with i.MX6 reference board (e.g. SARBE SD Board) to make sure the JTAG Tool and Test sequence are correct.

2. For the RESET sequence

Please make sure the RESET signal from JTAG Tool (XJTAG link2) can drive the i.MX6 POR_B to low to reset the system.

3. For the JTAG Bus connection

Sometimes the longer trace design (e.g. place the JTAG interface on debug board) may impact to the JTAG connection, and a jumper wire to shorten the trace length (connect the JTAG connector to the CPU board directly) can solve it.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply

3,388 Views
vittoria98
Contributor I

Hello @riteshmpatel thanks for the reply, 

How do I check if the RESET signal from JTAG Tool (XJTAG link2) can drive the i.MX6 POR_B to low to reset the system?

Thank you, 

Vittoria

0 Kudos
Reply

3,374 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @vittoria98,

You can use Oscilloscope to monitor the RESET signal from JTAG Tool (XJTAG link2) and i.MX6 POR_B signal to check the RESET flow.

Thanks & Regards,
Ritesh M Patel

 

0 Kudos
Reply