IMX6Q: using parallel CSI on second IPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q: using parallel CSI on second IPU

2,350 Views
Selea
Senior Contributor I

I'm trying to use a parallel sensor on the second parallel CSI input. this second paralle (according with documentation) can be routed only on the second IPU.

so in my DTS i have IPU_id=1 and CSI_id=1.

the driver probe is working fine, the sensor is found , configured and the signal seems to be present and correct. the V4L2 device is created (/dev/video2) but when i try to read from it it sat read timeout...

Any suggestion.

Omar

Tags (2)
0 Kudos
Reply
3 Replies

1,939 Views
fabio_estevam
NXP Employee
NXP Employee

Time to start a new thread?

0 Kudos
Reply

1,939 Views
Selea
Senior Contributor I

maybe yes, anyway i will attach the new DTS files that make USB H1 and USB OTG working on  phyflex

0 Kudos
Reply

1,939 Views
Selea
Senior Contributor I

I add my DTS files (they are customized for our board startting from phytec one). As you will see I addedd a Cmos sensor AR0134 that shoul use the parallel input port on the second IPU.

and i configured the second paralle port pins as well.

The driver is loaded, the sensor is configured on I2C, and i see the device created, but when i try to read from that one it not works : just say timeout... seems that the port is not capturing

so i think i missing some initialization on CSI or IPU.

0 Kudos
Reply