IMX6Q usb HOST

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q usb HOST

1,366 次查看
小辉哥
Contributor III

imx6q 识别不了U盘,接上usb鼠标可以识别到:

pastedImage_2.png

PCB一定要做90欧的阻抗吗?这个大概是什么原因导致的呢?

标签 (2)
0 项奖励
回复
1 回复

1,193 次查看
igorpadykov
NXP Employee
NXP Employee

Q[translated by Google]:

imx6q can not identify U disk, then usb mouse can be identified:
PCB must do 90 ohm impedance? What is the reason for this?

A:

Hi  小辉哥

yes reason may be poor signal, note mouse is detected as low speed device.

One can look at AN4589 Configuring USB on i.MX6 Series Processors 

sect.4.3.3 Operational settings for settings to tweak signal

https://cache.nxp.com/docs/en/application-note/AN4589.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复