IMX6Q system hang-up problem / linux kernel(3.0.35)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q system hang-up problem / linux kernel(3.0.35)

30,781 Views
raoxd
Contributor II

hi

     imx6q use L3.0.35_4.1.0_130816 to build u-boot,kernel and rootfs.  when we run our app(qt app), the system hang-up when run 3 days. it happen serval times.

     in the kernel log you may find notifications like:

     [ 73.247613] INFO: rcu_preempt_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=6002 jiffies)
     [   77.257610] INFO: rcu_bh_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=6002 jiffies)
     [  253.567611] INFO: rcu_preempt_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=24034 jiffies)
     [  257.577611] INFO: rcu_bh_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=24034 jiffies)
     [  433.887610] INFO: rcu_preempt_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=42066 jiffies)
     [  437.897611] INFO: rcu_bh_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=42066 jiffies)
     [  614.207612] INFO: rcu_preempt_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=60098 jiffies)
     [  618.217610] INFO: rcu_bh_state detected stalls on CPUs/tasks: { 0} (detected by 3, t=60098 jiffies)

     

    in community, i find someone encounter the same problem,according Re: Re: freescale android kernel have scheduling problem !!!,i follow steps below to patch my kernel.

    1.modify time.c

rcu_preempt_state detected stalls" could be fixed with the followng patch, please try

--- linux-3.0.35/arch/arm/plat-mxc/time.c.orig2013-12-11 09:25:29.518910709 +1300
+++ linux-3.0.35/arch/arm/plat-mxc/time.c2013-12-11 09:26:12.958912361 +1300

@@ -165,7 +165,8 @@

__raw_writel(tcmp, timer_base + V2_TCMP);

-return 0;

+        return evt < 0x7fffffff &&

+            (int)(tcmp - __raw_readl(timer_base + V2_TCN)) < 0 ? ETIME : 0;

}

#ifdef DEBUG

   2.patch 0027-ENGR00306276-iMX6-Add-workaround-for-ARM-errata-7613.patch, 0026-ENGR00306257-1027-fix-system-hang-up-issue-caused-by.patch and 0025-ENGR00295714-GPT-Status-register-bits-are-cleared-in.patch

   but when i finish modify,the kernel still hung up like before。 i also try to update gpu lib to p13,but i found lib(libEGL,libGAL) in gpu-viv-bin-mx6q-3.0.35-4.1.0 can not work in p13. is it p13 cannot used in linux?

   is there anyting  i can try to fix this problem in linux?

Labels (2)
34 Replies

7,399 Views
wallyyeh
Contributor V

Hi, igorpadykov:

    I also focus on this potential issue, could you provide the link of these patches for old SDK-3.0.35-4.1.0?

0 Kudos
Reply

6,534 Views
igorpadykov
NXP Employee
NXP Employee

patch will be released soon on official i.MX6 site.

0 Kudos
Reply

6,534 Views
raoxd
Contributor II

Hi igorpadykov:

     what you meant is that freescal will release new version for Linux3.0.35 this week, or just release some patch?

     it will be released by SABRE Board Reference Design|Freescale?

    

     if no,please give me link to download when released.We are in urgent need of this patch。thanks.

0 Kudos
Reply

6,534 Views
PeterChan
NXP Employee
NXP Employee

I have picked up some recent bug fixes for L3.0.35_4.1.0 that may related to this hang up issue. Would you please apply these patches in sequence and let me know if the problem still persists?

Note: 0009-ARM-imx-return-zero-in-case-next-event-gets-a-large-.patch is added

0 Kudos
Reply

6,534 Views
simon_cai
Contributor III

Hi PeterChan

I also meet hand up issue on android 4.2.2 BSP.

can I take use of your attached patch files to merge into Android 4.2.2 BSP??

does Android 4.2.2 BSP kernel version is base on L3.0.35_4.1.0  ???

0 Kudos
Reply

6,534 Views
raoxd
Contributor II

Hi,PeterChan:

     i have patch the file what you provide.i have test for serval days.but The problem still persists.

     i found that, the patch you provide can delay error happen,but cannot fix it.

     is there anyting i can try ? thanks!

    

0 Kudos
Reply

6,534 Views
PeterChan
NXP Employee
NXP Employee

Has the board pass the DDR stress test at https://community.freescale.com/docs/DOC-96412?

Have you ever checked the i.MX6 input power rails to ensure they can meet the minimum voltage requirement?

The L3.0.101_4.1.1 has just released at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab. Could you please try this release?

0 Kudos
Reply

6,534 Views
raoxd
Contributor II

Hi,PeterChan:

     i has run DDR stress test, and pass when i set freq from 450MHZ to 672MHZ.

     and input power also can meet the minimum voltage requirment.

     i has try L3.0.101_4.1.1,the problem still  persists, it just like L3.0.35_4.1.0 when patch file what you supply.

     compare to L3.0.35_4.1.0,  i found that L3.0.101_4.1.1(or L3.0.35_4.1.0 with patch) just printf the log(rcu_preempt_state detected stalls...),but the system did not hang up.

     it also did not printf log Frequently.

0 Kudos
Reply

6,534 Views
igorpadykov
NXP Employee
NXP Employee

patches released on link below several days ago

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

IMX6_JB43_111_ANDROID_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Android BSP Source Code Files.  Modified: 10/24/2014


0 Kudos
Reply

6,534 Views
simon_cai
Contributor III

Hi igorpadykov

PeterChan

Thanks for you information about the "android_jb4.3_1.1.1-ga_source.tar"patch.

As what I understand, this jb4.3_1.1.1 patch is just for FSL Android 4.3 version.

while, what about FSL Android 4.4.2 BSP version??does this version need to do the patch??

FSL didnot release any patch about Android 4.4.2 on the official imx6 site ,

could i think that FSL Android 4.4.2 BSP have been merged all these patch?

0 Kudos
Reply

6,534 Views
igorpadykov
NXP Employee
NXP Employee

Hi cai

yes android 4.4.2 also needs these patches, though

I do not know when they will be released.

~igor

0 Kudos
Reply

6,534 Views
simon_cai
Contributor III

hi igorpadykov

thanks for your relay.

one more question, Can Android 4.2.2 BSP be taking use of these Patchs(android_jb4.3_1.1.1-ga_source.tar)??

0 Kudos
Reply

6,534 Views
igorpadykov
NXP Employee
NXP Employee

Android 4.2.2 uses L3.0.35_4.0.0 while jb4.3_1.1

L3.0.35_4.1.0, probably some modifications are needed.

0 Kudos
Reply

6,534 Views
wallyyeh
Contributor V

It take me more than 5 minutes to get the link, here is the correct position which igorpadykov provide:

1. enter the web page:

    http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

2. In "Run-time software (70) Expand All"   <-- notice (70) might increse to (71) or more

    click the sub class "Operating System Software-Board Support Packages (30) "   <-- notice (30) might increse to (31) or more

3. click "IMX6_JB43_111_ANDROID_SOURCE_BSP", now you can download the file.

cheers

0 Kudos
Reply