IMX6Q processor WDOG output pin configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q processor WDOG output pin configuration

2,416 Views
vinodkumar
Contributor I

Hi all,

we are using IMX6Q processor in our design.

we are using Watch dog output pin to reset PMIC.

As per reference manual, it is configured to GPIO1_9 & GPIO1_1.


But in our board it is connected to GPIO1_3. see attached schematic.


In IMX6Q datasheet, note showing that "WDOG1_B output signals (for each one of the Watchdog modules) do not have dedicated pins, but are muxed out through the IOMUX. See the IOMUX manual for detailed information." see attached



Please let us know this watch dog timer output can be configured to GPIO1_3

Labels (1)
0 Kudos
Reply
1 Reply

2,272 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinod

GPIO_3 has not option for WDOG output, please check attached part of RM

i.MX6DQ Reference Manual (rev.2  7/2014)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

0 Kudos
Reply