IMX6Q first start boot fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q first start boot fail

2,115 Views
tommyduan
Contributor III

IMX6第一次上电启动不了,我们用的是IMX6Q,在所有电断开一段时间后,有两块板子出现第一次启动不了!串口也没打印信息!后来测试发现RTC晶振这里有影响,我只要示波器点击晶振的IN或者飞线出来就可以正常启动,但是测试晶振也是震荡没问题的,为啥这里受影响?我将晶振的IN给短接到地也可以启动,更改晶振的匹配电容没用!不知道具体哪里原因引起启动异常!异常时候我再立刻上电就可以起来或者对CPU复位也可以起来,放置久就不行!我从量时序和BOOT配置没发现有明显异常?帮忙给下分析思路,谢谢!

Labels (3)
Tags (1)
0 Kudos
Reply
3 Replies

1,928 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Tommy,

     You can try like below:

1. Populated 10M resistor between IN and OUT of CPU Cystal PIN.

or

2. Remove 32.768K crystal , 2 capacitors and 10M resistor.

Try it please!

Best Regards,

TIC Weidong

0 Kudos
Reply

1,928 Views
tommyduan
Contributor III

你好,问一个问题,32.768K晶振在系统启动过程主要啥作用?如果这个晶振异常是否影响系统启动?另外在时序要求没看到对这个晶振要求,是否要求在por拉高之前也要保证这个晶振稳定?如果外部晶振稳定时间较长,启动时候是否用内部晶振?另外6Q的内部晶振稳定需要多长时间?目前我有个6Q项目,有两台启动不了,发现跟这个32.768晶振有关?能否给出详细解释,和验证思路?谢谢!

0 Kudos
Reply

1,928 Views
tommyduan
Contributor III

Thanks your relay!

    1、Two pieces of bad,one pcs is OK  we Populated 2M resistor between IN and OUT of CPU Cystal PIN;The other one goes your way,Populated 10M resistor between IN and OUT of CPU Cystal PIN.it still can't start first!

    2、I remove RTC CLK,it's OK!

Can you tell me the really reason,or What experiments we need to do?To avoid this problem in the future!

 

Best Regards

0 Kudos
Reply