IMX6Q error during u-boot load

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q error during u-boot load

4,019件の閲覧回数
rage
Contributor I

Hi all,

I'm trying to start a Digi CC6 IMX6 into my hardware design.

The CPU reference is CC-WMX-J97C_TN-1.

I'm using usb imx tool to download u-boot file into the internal memory.

The connection between the PC containing the usb imx tool and the CPU is sucessful, but when I start uploading the u-boot, here is the error that i see :

config file <./imx_usb.conf>

vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf

vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf

vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf

vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x007d file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0076 file_name=mx7_usb_work.conf

vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf

vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf

vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf

vid=0x066f pid=0x37ff file_name=linux_gadget.conf

config file <./mx6_usb_work.conf>

parse ./mx6_usb_work.conf

15a2:0054(mx6_qsb) bConfigurationValue =1

Interface 0 claimed

HAB security state: development mode (0x56787856)

== work item

filename ../u-boot-imx6/u-boot.imx

load_size 0 bytes

load_addr 0x00000000

dcd 1

clear_dcd 0

plug 1

jump_mode 2

jump_addr 0x00000000

== end work item

Setting boot_data_ptr to 0

main dcd length 2f0

sub dcd length 2ec

loading binary file(../u-boot-imx6/u-boot.imx) to 177ffc00, skip=0, fsize=47d04 type=aa

out err=-7, last_trans=0 cnt=0x3c00 max=0x400 transferSize=0x400 retry=0

out err=-7, last_trans=0 cnt=0x3c00 max=0x200 transferSize=0x400 retry=1

out err=-7, last_trans=0 cnt=0x3c00 max=0x100 transferSize=0x400 retry=2

out err=-7, last_trans=0 cnt=0x3c00 max=0x80 transferSize=0x400 retry=3

out err=-7, last_trans=0 cnt=0x3c00 max=0x40 transferSize=0x400 retry=4

out err=-7, last_trans=0 cnt=0x3c00 max=0x20 transferSize=0x400 retry=5

out err=-7, last_trans=0 cnt=0x3c00 max=0x10 transferSize=0x400 retry=6

out err=-7, last_trans=0 cnt=0x3c00 max=0x8 transferSize=0x400 retry=7

out err=-7, last_trans=0 cnt=0x3c00 max=0x10 transferSize=0x400 retry=8

out err=-7, last_trans=0 cnt=0x3c00 max=0x8 transferSize=0x400 retry=9

out err=-7, last_trans=0 cnt=0x3c00 max=0x10 transferSize=0x400 retry=10

Giving up

HAB security state: development mode (0x00000000)

Do you know I can solve this issue ?

Thank you for your help.

Régis

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,286件の閲覧回数
kaa
Contributor II

I have the same problem, but by git bisect I found who broken the imx_usb Smiley Happy

commit 6deb910dd0a64267c43e65e95486f975e293823f

Author: Jeremie Corbier <[email protected]>
Date:   Tue Apr 19 10:58:06 2016 +0200

    Use the DCD_WRITE SDP command
    
    Signed-off-by: Jeremie Corbier <[email protected]>‍‍‍‍‍‍‍‍
0 件の賞賛
返信

3,286件の閲覧回数
tamilarasane
Contributor III

Hi I am also facing the same issue while doing otg boot in iMX6 Quad custom board. any one fixed this issue?

config file <./imx_usb.conf>

vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf

vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf

vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf

vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf

vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf

vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf

vid=0x066f pid=0x37ff file_name=linux_gadget.conf

config file <./mx6_usb_work.conf>

parse ./mx6_usb_work.conf

15a2:0054(mx6_qsb) bConfigurationValue =1

Interface 0 claimed

HAB security state: development mode (0x56787856)

== work item

filename u-boot.imx

load_size 0 bytes

load_addr 0x00000000

dcd 1

clear_dcd 0

plug 1

jump_mode 2

jump_addr 0x00000000

== end work item

main dcd length 308

sub dcd length 304

loading binary file(u-boot.imx) to 177fb000, skip=0, fsize=115174 type=aa

out err=-7, last_trans=0 cnt=0x4000 max=0x400 transferSize=0x0 retry=0

out err=-7, last_trans=0 cnt=0x4000 max=0x200 transferSize=0x0 retry=1

out err=-7, last_trans=0 cnt=0x4000 max=0x100 transferSize=0x0 retry=2

out err=-7, last_trans=0 cnt=0x4000 max=0x80 transferSize=0x0 retry=3

out err=-7, last_trans=0 cnt=0x4000 max=0x40 transferSize=0x0 retry=4

out err=-7, last_trans=0 cnt=0x4000 max=0x20 transferSize=0x0 retry=5

out err=-7, last_trans=0 cnt=0x4000 max=0x10 transferSize=0x0 retry=6

out err=-7, last_trans=0 cnt=0x4000 max=0x8 transferSize=0x0 retry=7

out err=-7, last_trans=0 cnt=0x4000 max=0x10 transferSize=0x0 retry=8

out err=-7, last_trans=0 cnt=0x4000 max=0x8 transferSize=0x0 retry=9

out err=-7, last_trans=0 cnt=0x4000 max=0x10 transferSize=0x0 retry=10

Giving up

HAB security state: development mode (0x00000000)

Thanks,

Tamilarasan

0 件の賞賛
返信

3,286件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Regis

I would suggest to ask on digi support for correct uboot image for

Digi CC6 IMX6 board:

Product Support - Digi International

usb loader usage is described on below links

https://github.com/boundarydevices/imx_usb_loader/blob/master/mx6_usb_work.conf

https://community.freescale.com/docs/DOC-94117

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信