IMX6Q and Nand flash interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q and Nand flash interface

1,096 Views
jk1z
Contributor I

Hi,

I have a question regarding a NAND flash device with spare area greater than 512bytes.

I have noted the IMX6 reference manual, it says that the spare area per page is 512 bytes.

So IMX6Q does not support NAND with spare area greater than 512 bytes? Kindly confirm.

regards

Labels (1)
0 Kudos
Reply
1 Reply

939 Views
igorpadykov
NXP Employee
NXP Employee

Hi jk

yes manual is correct: max spare area per page is 512 bytes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------