IMX6Q and Nand flash interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q and Nand flash interface

1,079 次查看
jk1z
Contributor I

Hi,

I have a question regarding a NAND flash device with spare area greater than 512bytes.

I have noted the IMX6 reference manual, it says that the spare area per page is 512 bytes.

So IMX6Q does not support NAND with spare area greater than 512 bytes? Kindly confirm.

regards

标签 (1)
0 项奖励
回复
1 回复

922 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jk

yes manual is correct: max spare area per page is 512 bytes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------