i.MX8M can do hardware scaling?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M can do hardware scaling?

1,154 Views
george
Senior Contributor II

Dear all,

i.MX8M does not have 2D-GPU.

      *This table is an excerpt from i.MX Graphics User’s Guide, Rev. 2, 04/2019.

pastedImage_3.png

 

For example, when scaling and displaying a movie, I guess to use DCSS.

Does the current BSP(L4.14.98_2.0.0_ga) support it?

Please let me know if there are any notes or limitations in using gstreamer or sink as compared to i.MX series with other 2D-GPU.

Best Regards,

George

Labels (1)
0 Kudos
Reply
1 Reply

1,041 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  yes, the DCSS may be used for scaling:

use section 7 (Multimedia) of "i.MX_Linux_Release_Notes.pdf" and section 6.3.5 [Display

Control Subsystem (DCSS)] of ''i.MX_Reference_Manual.pdf".

https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga 

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply