IMX6Q PWM frequency is not correct

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q PWM frequency is not correct

2,987 Views
zhongjiansun
Contributor I

hi,

   I have a problem with imx6q pwm. 

I use 

echo 0 >/sys/class/pwm/pwmchip1/export

echo 100 >/sys/class/pwm/pwmchip1/pwm0/period

echo 50 >/sys/class/pwm/pwmchip1/pwm0/duty_cycle

echo 1 >/sys/class/pwm/pwmchip1/pwm0/enable

I set pwm period is 100ns, duty_cycle 50ns, means that the pwm frequency is 10MHz, duty is 50%, but the oscilloscope shows the pwm frequency is 11MHz, and when the period is 92-100, the frequency is always 11MHz, when the period is 90, the frequency is 13.2MHz. 

why is that? I check the pwm clock ,is 66MHz.

Labels (1)
0 Kudos
Reply
4 Replies

2,611 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Zhongjiang,

I assume you are using a custom board, is that correct? What BSP are you using?

Regards,

Carlos

0 Kudos
Reply

2,611 Views
zhongjiansun
Contributor I

Hi Carlos,

     Yes, I designed a custom board. And I use L3.14.5.

     Depends on my project, I need GPIO1 to output a 12MHz, 50% square wave.

     Here is the pwm driver. I found there is no imx6 in this file, but imx6 pwm register offset address is the same as imx27, so I assume it's fine.

/*
* simple driver for PWM (Pulse Width Modulator) controller
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
* Derived from pxa PWM driver by eric miao <eric.miao@marvell.com>
*/

#include <linux/module.h>
#include <linux/kernel.h>
#include <linux/platform_device.h>
#include <linux/slab.h>
#include <linux/err.h>
#include <linux/clk.h>
#include <linux/delay.h>
#include <linux/io.h>
#include <linux/pwm.h>
#include <linux/of.h>
#include <linux/of_device.h>

/* i.MX1 and i.MX21 share the same PWM function block: */

#define MX1_PWMC 0x00 /* PWM Control Register */
#define MX1_PWMS 0x04 /* PWM Sample Register */
#define MX1_PWMP 0x08 /* PWM Period Register */

#define MX1_PWMC_EN (1 << 4)

/* i.MX27, i.MX31, i.MX35 share the same PWM function block: */

#define MX3_PWMCR 0x00 /* PWM Control Register */
#define MX3_PWMSR 0x04 /* PWM Status Register */
#define MX3_PWMSAR 0x0C /* PWM Sample Register */
#define MX3_PWMPR 0x10 /* PWM Period Register */
#define MX3_PWMCR_PRESCALER(x) ((((x) - 1) & 0xFFF) << 4)
#define MX3_PWMCR_DOZEEN (1 << 24)
#define MX3_PWMCR_WAITEN (1 << 23)
#define MX3_PWMCR_DBGEN (1 << 22)
#define MX3_PWMCR_CLKSRC_IPG_HIGH (2 << 16)
#define MX3_PWMCR_CLKSRC_IPG (1 << 16)
#define MX3_PWMCR_SWR (1 << 3)
#define MX3_PWMCR_EN (1 << 0)
#define MX3_PWMSR_FIFOAV_4WORDS 0x4
#define MX3_PWMSR_FIFOAV_MASK 0x7

#define MX3_PWM_SWR_LOOP 5

struct imx_chip {
struct clk *clk_per;
struct clk *clk_ipg;

void __iomem *mmio_base;

struct pwm_chip chip;

int (*config)(struct pwm_chip *chip,
struct pwm_device *pwm, int duty_ns, int period_ns);
void (*set_enable)(struct pwm_chip *chip, bool enable);
};

#define to_imx_chip(chip) container_of(chip, struct imx_chip, chip)

static int imx_pwm_config_v1(struct pwm_chip *chip,
struct pwm_device *pwm, int duty_ns, int period_ns)
{
struct imx_chip *imx = to_imx_chip(chip);

/*
* The PWM subsystem allows for exact frequencies. However,
* I cannot connect a scope on my device to the PWM line and
* thus cannot provide the program the PWM controller
* exactly. Instead, I'm relying on the fact that the
* Bootloader (u-boot or WinCE+haret) has programmed the PWM
* function group already. So I'll just modify the PWM sample
* register to follow the ratio of duty_ns vs. period_ns
* accordingly.
*
* This is good enough for programming the brightness of
* the LCD backlight.
*
* The real implementation would divide PERCLK[0] first by
* both the prescaler (/1 .. /128) and then by CLKSEL
* (/2 .. /16).
*/
u32 max = readl(imx->mmio_base + MX1_PWMP);
u32 p = max * duty_ns / period_ns;
writel(max - p, imx->mmio_base + MX1_PWMS);

return 0;
}

static void imx_pwm_set_enable_v1(struct pwm_chip *chip, bool enable)
{
struct imx_chip *imx = to_imx_chip(chip);
u32 val;

val = readl(imx->mmio_base + MX1_PWMC);

if (enable)
val |= MX1_PWMC_EN;
else
val &= ~MX1_PWMC_EN;

writel(val, imx->mmio_base + MX1_PWMC);
}

static int imx_pwm_config_v2(struct pwm_chip *chip,
struct pwm_device *pwm, int duty_ns, int period_ns)
{
struct imx_chip *imx = to_imx_chip(chip);
struct device *dev = chip->dev;
unsigned long long c;
unsigned long period_cycles, duty_cycles, prescale;
unsigned int period_ms;
bool enable = test_bit(PWMF_ENABLED, &pwm->flags);
int wait_count = 0, fifoav;
u32 cr, sr;

/*
* i.MX PWMv2 has a 4-word sample FIFO.
* In order to avoid FIFO overflow issue, we do software reset
* to clear all sample FIFO if the controller is disabled or
* wait for a full PWM cycle to get a relinquished FIFO slot
* when the controller is enabled and the FIFO is fully loaded.
*/
if (enable) {
sr = readl(imx->mmio_base + MX3_PWMSR);
fifoav = sr & MX3_PWMSR_FIFOAV_MASK;
if (fifoav == MX3_PWMSR_FIFOAV_4WORDS) {
period_ms = DIV_ROUND_UP(pwm->period, NSEC_PER_MSEC);
msleep(period_ms);

sr = readl(imx->mmio_base + MX3_PWMSR);
if (fifoav == (sr & MX3_PWMSR_FIFOAV_MASK))
dev_warn(dev, "there is no free FIFO slot\n");
}
} else {
writel(MX3_PWMCR_SWR, imx->mmio_base + MX3_PWMCR);
do {
usleep_range(200, 1000);
cr = readl(imx->mmio_base + MX3_PWMCR);
} while ((cr & MX3_PWMCR_SWR) &&
(wait_count++ < MX3_PWM_SWR_LOOP));

if (cr & MX3_PWMCR_SWR)
dev_warn(dev, "software reset timeout\n");
}

c = clk_get_rate(imx->clk_per);
c = c * period_ns;
do_div(c, 1000000000);
period_cycles = c;

prescale = period_cycles / 0x10000 + 1;

period_cycles /= prescale;
c = (unsigned long long)period_cycles * duty_ns;
do_div(c, period_ns);
duty_cycles = c;

/*
* according to imx pwm RM, the real period value should be
* PERIOD value in PWMPR plus 2.
*/
if (period_cycles > 2)
period_cycles -= 2;
else
period_cycles = 0;

writel(duty_cycles, imx->mmio_base + MX3_PWMSAR);
writel(period_cycles, imx->mmio_base + MX3_PWMPR);

cr = MX3_PWMCR_PRESCALER(prescale) |
MX3_PWMCR_DOZEEN | MX3_PWMCR_WAITEN |
MX3_PWMCR_DBGEN | MX3_PWMCR_CLKSRC_IPG_HIGH;

if (enable)
cr |= MX3_PWMCR_EN;

writel(cr, imx->mmio_base + MX3_PWMCR);

return 0;
}

static void imx_pwm_set_enable_v2(struct pwm_chip *chip, bool enable)
{
struct imx_chip *imx = to_imx_chip(chip);
u32 val;

val = readl(imx->mmio_base + MX3_PWMCR);

if (enable)
val |= MX3_PWMCR_EN;
else
val &= ~MX3_PWMCR_EN;

writel(val, imx->mmio_base + MX3_PWMCR);
}

static int imx_pwm_config(struct pwm_chip *chip,
struct pwm_device *pwm, int duty_ns, int period_ns)
{
struct imx_chip *imx = to_imx_chip(chip);
int ret;

ret = clk_prepare_enable(imx->clk_ipg);
if (ret)
return ret;

ret = imx->config(chip, pwm, duty_ns, period_ns);

clk_disable_unprepare(imx->clk_ipg);

return ret;
}

static int imx_pwm_enable(struct pwm_chip *chip, struct pwm_device *pwm)
{
struct imx_chip *imx = to_imx_chip(chip);
int ret;

ret = clk_prepare_enable(imx->clk_per);
if (ret)
return ret;

imx->set_enable(chip, true);

return 0;
}

static void imx_pwm_disable(struct pwm_chip *chip, struct pwm_device *pwm)
{
struct imx_chip *imx = to_imx_chip(chip);

imx->set_enable(chip, false);

clk_disable_unprepare(imx->clk_per);
}

static struct pwm_ops imx_pwm_ops = {
.enable = imx_pwm_enable,
.disable = imx_pwm_disable,
.config = imx_pwm_config,
.owner = THIS_MODULE,
};

struct imx_pwm_data {
int (*config)(struct pwm_chip *chip,
struct pwm_device *pwm, int duty_ns, int period_ns);
void (*set_enable)(struct pwm_chip *chip, bool enable);
};

static struct imx_pwm_data imx_pwm_data_v1 = {
.config = imx_pwm_config_v1,
.set_enable = imx_pwm_set_enable_v1,
};

static struct imx_pwm_data imx_pwm_data_v2 = {
.config = imx_pwm_config_v2,
.set_enable = imx_pwm_set_enable_v2,
};

static const struct of_device_id imx_pwm_dt_ids[] = {
{ .compatible = "fsl,imx1-pwm", .data = &imx_pwm_data_v1, },
{ .compatible = "fsl,imx27-pwm", .data = &imx_pwm_data_v2, },
{ /* sentinel */ }
};
MODULE_DEVICE_TABLE(of, imx_pwm_dt_ids);

static int imx_pwm_probe(struct platform_device *pdev)
{
const struct of_device_id *of_id =
of_match_device(imx_pwm_dt_ids, &pdev->dev);
const struct imx_pwm_data *data;
struct imx_chip *imx;
struct resource *r;
int ret = 0;

if (!of_id)
return -ENODEV;

imx = devm_kzalloc(&pdev->dev, sizeof(*imx), GFP_KERNEL);
if (imx == NULL) {
dev_err(&pdev->dev, "failed to allocate memory\n");
return -ENOMEM;
}

imx->clk_per = devm_clk_get(&pdev->dev, "per");
if (IS_ERR(imx->clk_per)) {
dev_err(&pdev->dev, "getting per clock failed with %ld\n",
PTR_ERR(imx->clk_per));
return PTR_ERR(imx->clk_per);
}

imx->clk_ipg = devm_clk_get(&pdev->dev, "ipg");
if (IS_ERR(imx->clk_ipg)) {
dev_err(&pdev->dev, "getting ipg clock failed with %ld\n",
PTR_ERR(imx->clk_ipg));
return PTR_ERR(imx->clk_ipg);
}

imx->chip.ops = &imx_pwm_ops;
imx->chip.dev = &pdev->dev;
imx->chip.base = -1;
imx->chip.npwm = 1;
imx->chip.can_sleep = true;

r = platform_get_resource(pdev, IORESOURCE_MEM, 0);
imx->mmio_base = devm_ioremap_resource(&pdev->dev, r);
if (IS_ERR(imx->mmio_base))
return PTR_ERR(imx->mmio_base);

data = of_id->data;
imx->config = data->config;
imx->set_enable = data->set_enable;

ret = pwmchip_add(&imx->chip);
if (ret < 0)
return ret;

platform_set_drvdata(pdev, imx);
return 0;
}

static int imx_pwm_remove(struct platform_device *pdev)
{
struct imx_chip *imx;

imx = platform_get_drvdata(pdev);
if (imx == NULL)
return -ENODEV;

return pwmchip_remove(&imx->chip);
}

static struct platform_driver imx_pwm_driver = {
.driver = {
.name = "imx-pwm",
.owner = THIS_MODULE,
.of_match_table = imx_pwm_dt_ids,
},
.probe = imx_pwm_probe,
.remove = imx_pwm_remove,
};

module_platform_driver(imx_pwm_driver);

MODULE_LICENSE("GPL v2");
MODULE_AUTHOR("Sascha Hauer <s.hauer@pengutronix.de>");

0 Kudos
Reply

2,610 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi,

you mean L3.14.52_1.1.0_ga, is this correct? You can check PWM Driver in chapter 48 on the Linux reference Manual (attached). You must also check that general clock settings and that PWM registers are being configured correctly.


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,610 Views
zhongjiansun
Contributor I

Hi,

     I check the pwm clock setting in .dts file, it shows that:

  pwm@02084000 {
            #pwm-cells = <0x2>;
            compatible = "fsl,imx6q-pwm", "fsl,imx27-pwm";
            reg = <0x2084000 0x4000>;
            interrupts = <0x0 0x54 0x4>;
            clocks = <0x2 0x3e 0x2 0x92>;
            clock-names = "ipg", "per";
            pinctrl-names = "default";
            pinctrl-0 = <0x11>;
            status = "okay";
            linux,phandle = <0x4d>;
            phandle = <0x4d>;
};

       I couldn't understand what "clocks = <0x2 0x3e 0x2 0x92>" means. Could you explain it?

       Thank you very very much!

Regards,
Zhongjian

0 Kudos
Reply