IMX6Q MfgTool burn program failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q MfgTool burn program failed

2,498件の閲覧回数
tommyduan
Contributor III

We use Mfgtool burn program ,it stop"jumping to os image",can't going on!How can we find the reason?before it's ok,Where should I look for the reason?How does the burning process run?How does the system process work after startup?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,289件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tommy

stop"jumping to os image" may mean that board can not run mfg tool

since ddr settings are wrong for that board. It s necessary to run ddr test

i.MX6/7 DDR Stress Test Tool V2.92 

https://community.nxp.com/docs/DOC-328258 

and rebuild mfg tool with new ddr settings found from ddr test.

For example one can look on

How to build MFG Firmware for i.MX6Q 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信