IMX6Q Kernel Version V4.1.15

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Kernel Version V4.1.15

1,903 Views
shalanyang
Contributor II

we are using IMX6Q, why the NXP latest kernel version is 4.1.15,according to the kernel naming rules,  the kernel version is 4.x.y ,if the second number is odd number ,means the kernel version is developing and is not stable version,

could you tell why you are select the 4.1.15 as the base version?TKS!

Labels (3)
0 Kudos
Reply
2 Replies

1,750 Views
joanxie
NXP TechSupport
NXP TechSupport

" the kernel version is 4.x.y ,if the second number is odd number ,means the kernel version is developing and is not stable version" where did you get this information?

0 Kudos
Reply

1,750 Views
shalanyang
Contributor II

Hi ,joan

            I get the infomation from book,I think get the error information, I think I find the correct answer form

            Linux kernel - Wikipedia ," The even-odd system of alternation between stable and unstable was gone. Instead,

            development pre-releases are titled release candidates", thanks!

0 Kudos
Reply