IMX6Q- Ibis model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q- Ibis model

1,684件の閲覧回数
udayakumarr
Contributor I

Regarding I.MX 6Q,

In one the development boards  the I.MX 6Q and xilinx artis 7 series FPGA are used and both are connected thru PCIe Gen2 bus. We would like to have SI simulation for same. But, In the IBIS of I.MX, the PCIe pins are named as 'NC'. Can anyone help us to get fully enabled ( PCIe Bus) IBIS for IMX6 device.

Regards,

Udaya

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,465件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Udaya

please check sect.9.5.6 List of pins not modeled in the i.MX6 IBIS file

(PCIe among them) i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信