IMX6Q EMMC Flash is not working Android 9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q EMMC Flash is not working Android 9

1,469件の閲覧回数
laulavanya
Contributor II

Hi NXP,

Sdcard flash is working for android 9

Emmc :
Able to flash the binaries using uuu tool but unable to boot.

Facing below issue 

Can somebody identify quickly?

MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

Failed (-5)
No panel detected: default to ConsoleUI-XGA
Display: ConsoleUI-XGA (1280x800)
In: serial
Out: serial
Err: serial
flash target is MMC:1
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 1 not supported
Net: No ethernet found.
MMC: no card present
Block device mmc 1 not supported
bcb_rw_block, get_block_size return 0
read_bootctl, bcb_rw_block read failed
read command failed
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
cannot get the partion info for fbmisc
fastboot_get_lock_stat: error in get mmc part
MMC: no card present
fsl_read_from_partition_multi: mmc device not found
MMC: no card present
fsl_read_from_partition_multi: mmc device not found
avb_slot_verify.c:603: ERROR: boot: Error loading footer.

ラベル(2)
0 件の賞賛
返信
1 返信

1,452件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello laulavanya,

The Android 9 BSP doesn't work with i.MX6Q, it use the 64 bit only for compilation and deployment, you have to use the Android 8, or go to the community bsp.

 

Regards

 

0 件の賞賛
返信