IMX6Q Android8.0 Run Termux error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Android8.0 Run Termux error

2,663 Views
leavs
Contributor IV

Hi,

I have one custom device, I port the Android 8.0 system for my IMX6Q board.  Every thing is Ok, but When I running termux 0.65, there is some issue.

If I call termux-chroot command, I get:

```

10-17 00:15:07.624 2166-2166/? A/DEBUG: *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
10-17 00:15:07.624 2166-2166/? A/DEBUG: Build fingerprint: 'unknown'
10-17 00:15:07.624 2166-2166/? A/DEBUG: Revision: 'unknown'
10-17 00:15:07.624 2166-2166/? A/DEBUG: ABI: 'arm'
10-17 00:15:07.625 2166-2166/? A/DEBUG: pid: 2166, tid: 2166, name: /bin/bash >>> bash <<<
10-17 00:15:07.625 2166-2166/? A/DEBUG: signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0x0
10-17 00:15:07.625 2166-2166/? A/DEBUG: Cause: null pointer dereference
10-17 00:15:07.628 2166-2166/? A/DEBUG: r0 00000000 r1 7062d20f r2 00000000 r3 80000000
10-17 00:15:07.628 2166-2166/? A/DEBUG: r4 ad5af868 r5 7062d20f r6 00000018 r7 ad58c91d
10-17 00:15:07.628 2166-2166/? A/DEBUG: r8 bec21703 r9 00080000 sl bec21702 fp bec21708
10-17 00:15:07.628 2166-2166/? A/DEBUG: ip ad5ad63c sp bec21890 lr ad58cd5f pc ad53d9bc cpsr 600f0030
10-17 00:15:07.633 2166-2166/? A/libc: stack corruption detected (-fstack-protector)

```

Did anyone knows this problem?

Can anyone test this app in IMX6QDLEVB?

I install termux 0.65, and run follow command in termux 0.65:

```

$ pkg install proot

$ termux-chroot

```

Labels (1)
0 Kudos
Reply
3 Replies

2,445 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot help you with this problem since Termux is not supported by us. I apologize for the inconveniences.

Best Regards,

Diego.

0 Kudos
Reply

2,445 Views
leavs
Contributor IV

Thanks for your reply. Do you know another bug for Ethernet App from NXP?

Please check:

https://community.nxp.com/thread/487110 

0 Kudos
Reply

2,445 Views
leavs
Contributor IV

Is everyone know this problem?

0 Kudos
Reply