IMX6DUAL IPU ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DUAL IPU ERROR

2,805 Views
alessandroinnoc
Contributor II

Hi to all !

I got a strange behavior on my IMX6D using kernel 3.14.38;. The main application generates a rtp stream using  imxvpuenc_h264 element of gstreamer-1.0 framework. Once this application started, any access to the IPU, for istance using the imxipuvideosink element, is not possible.

The kernel's log shows the following messages:

[  433.836103] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x02000000

[  434.814092] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0x80 "wait_for_comp_timeout" ret:0,line:2964

[  435.794088] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0x90 "wait_for_comp_timeout" ret:0,line:2964

[  436.774091] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0xa0 "wait_for_comp_timeout" ret:0,line:2964

[  437.754086] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0xb0 "wait_for_comp_timeout" ret:0,line:2964

[  452.664097] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0xc0 "wait_for_comp_timeout" ret:0,line:2964

[  453.644092] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0xd0 "wait_for_comp_timeout" ret:0,line:2964

[  454.624085] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0xe0 "wait_for_comp_timeout" ret:0,line:2964

[  455.604085] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0xf0 "wait_for_comp_timeout" ret:0,line:2964

[  456.594090] imx-ipuv3 2400000.ipu: ERR:[0x86b3b400]-no:0x100 "wait_for_comp_timeout" ret:0,line:2964

Does any one faced (and possibly solved) such error ?

Thanks a lot !

Alessandro Innocenti

Labels (1)
0 Kudos
Reply
1 Reply

2,567 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alessandro

could you try nxp bsp with gst1.0-fsl-plugins, please check

attached Release Notes Table 6, Linux Guide sect.7.3.10, found on

i.MX 6 Series Software and Development Tool|NXP

There are 2 separate plugin's : community GStreamer-imx plugins

(supported on meta-fsl-arm mailing list https://lists.yoctoproject.org/listinfo/meta-freescale )

and nxp GStreamer Plugins (fsl-gst-plugin package), difference between

nxp and community gstreamer 1.0 plugins :

trac.gateworks.com/wiki/Yocto/gstreamer

https://lists.yoctoproject.org/pipermail/meta-freescale/2014-August/010291.html

tutorial & examples

i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply