IMX6DQ Android6 Realtek RTL8188EU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DQ Android6 Realtek RTL8188EU

2,373 Views
先生孟
Contributor II

To NXP IMX6DQ Android Team:

    我们在IMX6Q Android 6.0上调试realtek的wifi 8188EUS模块,驱动已经加载,但是在进行无线连接的时候,出现以下错误

init: Starting service 'p2p_supplicant'...
init: Service 'p2p_supplicant' (pid 1132) exited with status 255
init: Starting service 'p2p_supplicant'...
init: Service 'p2p_supplicant' (pid 1141) exited with status 255
init: Starting service 'p2p_supplicant'...
init: Service 'p2p_supplicant' (pid 1149) exited with status 255
init: Starting service 'p2p_supplicant'...
init: Service 'p2p_supplicant' (pid 1156) exited with status 255
init: Starting service 'p2p_supplicant'...
init: Service 'p2p_supplicant' (pid 1175) exited with status 255
init: Starting service 'p2p_supplicant'...
init: Service 'p2p_supplicant' (pid 1182) exited with status 255

如果直接设置ifconfig wlan0 up ,wlan0可以挂载并且可以设置IP地址

RTL871X: +871x_drv - drv_open, bup=0
RTL871X: Set RF Chip ID to RF_6052 and RF type to 1T1R.
RTL871X: rtl8188e_FirmwareDownload fw:NIC, size: 13904
RTL871X: rtl8188e_FirmwareDownload: fw_ver=b fw_subver=0001 sig=0x88e1, Month=11, Date=27, Hour=30, Minute=36
RTL871X: polling_fwdl_chksum: Checksum report OK! (1, 0ms), REG_MCUFWDL:0x00030005
RTL871X: =====> _8051Reset88E(): 8051 reset success .
RTL871X: _FWFreeToGo: Polling FW ready OK! (21, 10ms), REG_MCUFWDL:0x000300c6
RTL871X: FWDL success. write_fw:1, 80ms
==> rtl8188e_iol_efuse_patch
RTL871X: pDM_Odm TxPowerTrackControl = 1
RTL871X: rtl8188eu_hal_init in 1200ms
RTL871X: hw_var_set_opmode()-2938 mode = 2
RTL871X: MAC Address = 14:6b:9c:a9:a1:87
RTL871X: -871x_drv - drv_open, bup=1
RTL871X: ==>rtw_ps_processor .fw_state(8)
RTL871X: ==>ips_enter cnts:1
RTL871X: nolinked power save enter
RTL871X: ===> rtw_ips_pwr_down...................

RTL871X: ====> rtw_ips_dev_unload...
RTL871X: usb_read_port_cancel
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_read_port_complete() RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0)
RTL871X: usb_write_port_cancel
RTL871X: ==> rtl8188eu_hal_deinit
RTL871X: bkeepfwalive(0)
RTL871X: SetHwReg8188EU: bMacPwrCtrlOn=0
RTL871X: <=== rtw_ips_pwr_down..................... in 170ms

 

如果ifconfig -a 可以看到wlan0 已经成功配置了IP地址,

但是p2p_supplicant 还是无法Init,出现上面的错误,请问这个问题应该会在什么引起的呢?

非常感谢!

Tony 

2019-01-18

Labels (1)
0 Kudos
Reply
1 Reply

2,009 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Linjin Meng,

    It seems that P2P service couldn't be normally started, you can refer to the porting steps described in the link, the engineer also use Realtek product.

USB wifi调试笔记 - 木花猫 - 博客园 

Have a nice day!

NXP TIC Weidong Sun

0 Kudos
Reply