IMX6DP with isl79987 and LVDS in split mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6DP with isl79987 and LVDS in split mode

ソリューションへジャンプ
1,002件の閲覧回数
vaudoitlaurent
Contributor IV

Hi,

we are working on a custom imx6DP board, with a LVDS screen (using 2 lvds bus in split mode), and an isl79987 video decoder.
Kernel is 4.19 from NXP, on which we have the isl79987 patch for the 4 channel feature.

For testing, we use gstreamer or the nxp test application, mxc_v4l_tvin.

When we display image from camera, we can see that the image is not perfect, some bloc of lines seems shifted from the previous one (cf picture).

If we force the isl79987 to display a test patter (on the same channel), then the image is correct (no block of lines shifted).


We made the same test on a Wandboard with imx6QP and a hdmi display, and we do not have the problem.


Would you have an idea on where to search for this problem?

Thans in advance for your help.

Regards

LaurentIMG_20200907_092030[1].jpg

1 解決策
985件の閲覧回数
vaudoitlaurent
Contributor IV

Hi,

it seems the problems comes from the quartz used for the isl, which is not perfectly stable

Regards

Laurent

 

元の投稿で解決策を見る

2 返答(返信)
978件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Great, thank you for sharing your solution

0 件の賞賛
返信
986件の閲覧回数
vaudoitlaurent
Contributor IV

Hi,

it seems the problems comes from the quartz used for the isl, which is not perfectly stable

Regards

Laurent