IMX6DL - upload uboot on secured device with MFGTools(UUU)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL - upload uboot on secured device with MFGTools(UUU)

659 Views
adrian_dusinski
Contributor II

I'm trying to upload signed uboot to closed device with uuu tool:

mx6_usb_work.conf:

/home/adrian/workspace/yocto-master/build/tmp/deploy/images/imx6dl/cst/u-boot/u-boot.imx:dcd
/home/adrian/workspace/yocto-master/build/tmp/deploy/images/imx6dl/cst/u-boot/u-boot-signed.imx:clear_dcd,jump header

But I still receive failed :

config file </opt/distro/3.0/sysroots/x86_64-sdk-linux/etc/imx-loader.d//mx6_usb_work.conf>
parse /opt/distro/3.0/sysroots/x86_64-sdk-linux/etc/imx-loader.d//mx6_usb_work.conf
Trying to open device vid=0x15a2 pid=0x0061
Interface 0 claimed
HAB security state: production mode (0x12343412)
== work item
filename /home/adrian/workspace/yocto-master/build/tmp/deploy/images/imx6dl/cst/u-boot/u-boot.imx
load_size 0 bytes
load_addr 0x00000000
dcd 1
clear_dcd 0
plug 1
jump_mode 0
jump_addr 0x00000000
== end work item
loading DCD table @0x910000

<<<792, 792 bytes>>>
succeeded (security 0x12343412, status 0x128a8a12)
clear dcd_ptr=0x11ffb02c
HAB security state: production mode (0x12343412)
== work item
filename /home/adrian/workspace/yocto-master/build/tmp/deploy/images/imx6dl/cst/u-boot/u-boot-signed-pad.imx
load_size 0 bytes
load_addr 0x00000000
dcd 0
clear_dcd 1
plug 0
jump_mode 3
jump_addr 0x00000000
== end work item
clear dcd_ptr=0x11ffb02c

loading binary file(/home/adrian/workspace/yocto-master/build/tmp/deploy/images/imx6dl/cst/u-boot/u-boot-signed-pad.imx) to 11ffb000, skip=0, fsize=54000 type=aa

<<<344064, 344064 bytes>>>
succeeded (security 0x12343412, status 0x88888888)
jumping to 0x11ffb000
failed (security 0x12343412, status 0x3318c000)

I found in uuu documentation that for Imx6dl it's required to remove DCD address:

adrian_dusinski_1-1649433074490.png


So because of that I added clear_dcd,jump header in mx6_usb_work.conf, I also tried manually remove the address from signed image but nothing changes.

 

Update:

Is it normal that dcd address is removed at all? I thought that the script removes this address only for signing but then it save it again. When I'm reading memory with jtag I can see that address is removed:

adrian_dusinski_0-1649689893516.png

 

My image

adrian_dusinski_1-1649689913767.png

 

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies