Hi community.
Our customer has below question.
Would you please teach me about XTALI and RTC_XTALI (Clock Inputs) DC Parameters.
There are Only provision supplies MHz clock from an external VIL/VIH-level provisions of XTALI and RTC_XTALI Terminal ?.
Crystal oscillator child connection is not eligible?
Because for input on probes, such as quartz, and varying load capacity, such as correct DC level measurement is difficult,.
已解决! 转到解答。
Hi Takashi
XTALI and RTC_XTALI (Clock Inputs) DC Parameters are given in
Table 22. XTALI and RTC_XTALI DC Parameters i.MX6SDL Datasheet (rev.5, 6/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf
If crystal is connected to these pins, then levels are undefined as its value is defined
by used crystal quality.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takashi
XTALI and RTC_XTALI (Clock Inputs) DC Parameters are given in
Table 22. XTALI and RTC_XTALI DC Parameters i.MX6SDL Datasheet (rev.5, 6/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf
If crystal is connected to these pins, then levels are undefined as its value is defined
by used crystal quality.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------