IMX6D Poor Ethernet Performance (UDP)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6D Poor Ethernet Performance (UDP)

2,847件の閲覧回数
npatel
Contributor III

Hi,

We are using an IMX6D on a custom board, running the 4.14.98 Linux Kernel released by NXP. The custom board also uses an AR8031 PHY, similar to the IMX6QSabreSD eval board. I am seeing poor UDP performance, with lots of lost datagrams when testing with iperf3. Performance varies when testing against different machines running Windows/or Linux with Gigabit interfaces. But for the case when testing against the IMX6SabreSD board (which happens to be the BEST case), in an isolated network, UDP RX rates are between 285-300 Mbps with about 25% loss, and UDP TX rates top out at 160 Mbps with minimal datagram loss (<.5%). I am aware of the ERRATA on the MAC block of the SOC (ERR004512), which essentially says that performance is limited to around 400 Mbps (TX + RX) combined. I am seeing this with TCP, as expected. However UDP is performing terribly. Any suggestions on how to increase UDP performance? At least enough to be in line with the ERRATA.

Thanks!

Neil

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,700件の閲覧回数
npatel
Contributor III

Hi Victor,

So this issue with poor UDP performance is Iperf3 related. Switching to Iperf2, and limiting the client UDP bandwidth so that it is inline with ERRATA ERR004512 ( -b 400M), UDP performance was as expected.

Thank you!

Neil

0 件の賞賛
返信

2,700件の閲覧回数
b36401
NXP Employee
NXP Employee

Yes. There are some issues with iperf3. So you can use iperf2 instead of iperf3.

0 件の賞賛
返信

2,700件の閲覧回数
b36401
NXP Employee
NXP Employee

Please make sure that everything is fine with the connection on hardware level. I mean wires, etc.
Also please note that is is processor bus is loaded with some other task in addition to networkig it may cause loss also.

0 件の賞賛
返信