How to support I2S communicate in L4.1.15

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to support I2S communicate in L4.1.15

1,417件の閲覧回数
guochgz
Contributor III

Hello:

      on my board, Lmx2571 is connected to the IMX6ULL's sai3.

      pastedImage_1.png

   I have followed this post:

   i.MX7Dual + SGTL5000 no data on SAI output 

   to added simple-audio-card on my baseline, but after do that , there is nothing show on my board.

   pastedImage_4.png

   my dts file is like this:

   pastedImage_6.png

   pastedImage_7.png

   pastedImage_8.png

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,339件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 国承 张

one can try "simple-audio-card" patch :

ARM: dts: imx6ul-14x14-evk: Add audio support - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,339件の閲覧回数
guochgz
Contributor III

thanks igor, I have solved this issue by add code in soc-util.c.

0 件の賞賛
返信