If i want the X-11 is supported on the IMX8mq, what needs to be done?
I tried to use xwayland to be compatible with X11, but it didn't work due to an EGL error.If i use Weston directly, his features are not powerful enough. Is there any other desktop system to support Wayland's , such as the genome. . .
Hi,
So sorry about that
You can see that in our newest BSP
• No X11 backend is supported in i.MX 8MQuad.• No Frame Buffer backend is supported in i.MX 8MQuad
Hope this can do help for you.
Have a nice day
Rita
We want a desktop system similar to xfce, kde and the like. Based on imx8mq, 4.14.78. Is there any solution?
we didn’t choose weston because it’s too simple.
Or if you want to try the ubuntu that our third party make:
https://boundarydevices.com/wiki/ubuntu-for-nitrogen8/