IMX6 with aptina image sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 with aptina image sensor

4,232件の閲覧回数
janr_
Contributor I

Hello,

We try to use an aptina image sensor ar0330 with the IMX6.

We took uboot and the linux kernel from the sabresd referenceboard.

How could we include the right driver for the image sensor?

Do we have to use modprobe?

Or do we have to inlcude in into the kernel during the build process?

Where can we find the driver for the image sensor?

- Jan

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

2,680件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jan,

About porting linux BSP to your board, you'd better refer to the document i.MX_6Dual6Quad_BSP_Porting_Guide.pdf. And about the structure of linux BSP you can see details in i.MX_6Dual6Quad_Linux_Reference_Manual.pdf.

Here I attach them for you. Hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信