IMX6 with aptina image sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 with aptina image sensor

4,282 次查看
janr_
Contributor I

Hello,

We try to use an aptina image sensor ar0330 with the IMX6.

We took uboot and the linux kernel from the sabresd referenceboard.

How could we include the right driver for the image sensor?

Do we have to use modprobe?

Or do we have to inlcude in into the kernel during the build process?

Where can we find the driver for the image sensor?

- Jan

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

2,730 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jan,

About porting linux BSP to your board, you'd better refer to the document i.MX_6Dual6Quad_BSP_Porting_Guide.pdf. And about the structure of linux BSP you can see details in i.MX_6Dual6Quad_Linux_Reference_Manual.pdf.

Here I attach them for you. Hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复