IMX6 ultralite processor Hardware Development Guide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 ultralite processor Hardware Development Guide

2,112件の閲覧回数
shwethanarayan
Contributor I

Hi Team,

 

In the image below (highlighted in blue) of the IMX6 ultralite processor Hardware Development Guide, the migration notes has a point on the PMIC_STBY_REQ output voltage. There, the MOSFET is told to be changed from Vgth< 1.3 to a Vgth<2.7V. Could you please tell a specific part number for the same. Please also tell me what is the voltage for the PMIC_STBY_REQ.

shwethanarayan_0-1610533245949.png

 

Regards

Shwetha

0 件の賞賛
返信
3 返答(返信)

2,098件の閲覧回数
shwethanarayan
Contributor I

Hi,

 

Thanks for proving the voltage of PMIC_STBY_REQ.

I think TO1.0 has the part number RYU002N05 for Q501 and Q701. May I know what is the part number used in TO1.1.

 

Regards

Shwetha

0 件の賞賛
返信

2,071件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

For Q501 and Q701, it's part number is RYU002N05,  We have not changed them. 

 

weidong

0 件の賞賛
返信

2,101件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

    1. PMIC_STBY_REQ's voltage reference is VDD_SNVS_IN, which is 3.0V.

    2. For Q501 and Q701, it's part number is RYU002N05, which is ROHM's MOSFET.

Hope this information is helpful to you.

Have a nice day!

B.R,

weidong

       

0 件の賞賛
返信