IMX6 sololite with Android 4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 sololite with Android 4.2

1,819件の閲覧回数
marco_sinig
Contributor I

Hi All,

Freescale has released a JB4.2.2 for IMX6 but IMX 6sololite is not included.

https://community.freescale.com/docs/DOC-94798

One problem could be the missing 3D GPU on the sololite.

Android requires the availability of open GL support, either in HW or SW. On 4.2 Open SW GL is currently not supported by Google.


One solution would be to port the open GL support from release 4.0. Saying that, I have no idea if this can be a nightmare and if the performances would be good enough.


Can anyone confirm that?


Do you know if there are other major changes that could block the porting of JB4.2 on sololite?


Thanks in Advance

Marco

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,328件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Marco,

Android 4.2.2.1 should be available by mid october for the Solo Lite.

Stay tuned to our website for it.

0 件の賞賛
返信