IMX6 sololite with Android 4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 sololite with Android 4.2

1,823 Views
marco_sinig
Contributor I

Hi All,

Freescale has released a JB4.2.2 for IMX6 but IMX 6sololite is not included.

https://community.freescale.com/docs/DOC-94798

One problem could be the missing 3D GPU on the sololite.

Android requires the availability of open GL support, either in HW or SW. On 4.2 Open SW GL is currently not supported by Google.


One solution would be to port the open GL support from release 4.0. Saying that, I have no idea if this can be a nightmare and if the performances would be good enough.


Can anyone confirm that?


Do you know if there are other major changes that could block the porting of JB4.2 on sololite?


Thanks in Advance

Marco

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,332 Views
SergioSolis
NXP Employee
NXP Employee

Hello Marco,

Android 4.2.2.1 should be available by mid october for the Solo Lite.

Stay tuned to our website for it.

0 Kudos
Reply