IMX6 ,secure booting using HAB for kernel image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 ,secure booting using HAB for kernel image

8,893件の閲覧回数
Deepu
Contributor III

Hi Freescale Support Team,

1.In Imx6 series processors,in order to make HAB to authenticate boot image (for eg: u-boot),we need to call HAB APIs from u-boot directly?.

2.How can I extend this secure booting feature for kernel Image?...For kernel image authentication also ,can i follow the same steps used for  signing the u-boot using CST tools .?.

3.Where should I include the authentation APIs in kernel to make HAB to authenticate the uImage?

ラベル(7)
4 返答(返信)

3,654件の閲覧回数
Yuri
NXP Employee
NXP Employee

The following are information sources :

“i.MX 6 Linux High Assurance Boot (HAB) User's Guide”

from Linux documentation.

https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_LINUXDOCS_BUNDLE&location=null

AN4581

“Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4”

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

i.MX Trust Architecture presentation :

https://community.freescale.com/servlet/JiveServlet/download/313957-255581/20-i.MX_TrustArchitecture...

1.

The recent document states, that HAB API may be called from:

- Boot ROM.

− Other boot stages.

−APIs used in U-Boot in this session are:

hab_status_t(*report_event)(hab_status_tstatus, uint32_t index, uint8_t *event, size_t*bytes)

hab_status_t(*report_status)(hab_config_t*config, hab_state_t*state)

2.

Kernel image may be checked by U-boot, as mentioned in “i.MX 6 Linux High Assurance Boot (HAB) User's Guide” :

“The second stage is the authentication of uImage by U-Boot. authenticate_image is called

by U-boot to verify uImage when executing bootm.”

3,653件の閲覧回数
satyadamarla
Contributor III

Hello Yuri,

authenticate_image, can this also be done for zImage?

Cheers,

Satya

0 件の賞賛
返信

3,654件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

> authenticate_image, can this also be done for zImage?

Yes.

Regards,

Yuri.

3,653件の閲覧回数
Deepu
Contributor III

Hi  Yuri ,

     Thanks a lot for your post .I have all documents except i.MX 6 Linux High Assurance Boot (HAB) User's Guide .This document is very helpfull .Thanks for your help.

0 件の賞賛
返信