IMX6 ,secure booting using HAB for kernel image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 ,secure booting using HAB for kernel image

7,906 次查看
Deepu
Contributor III

Hi Freescale Support Team,

1.In Imx6 series processors,in order to make HAB to authenticate boot image (for eg: u-boot),we need to call HAB APIs from u-boot directly?.

2.How can I extend this secure booting feature for kernel Image?...For kernel image authentication also ,can i follow the same steps used for  signing the u-boot using CST tools .?.

3.Where should I include the authentation APIs in kernel to make HAB to authenticate the uImage?

4 回复数

2,667 次查看
Yuri
NXP Employee
NXP Employee

The following are information sources :

“i.MX 6 Linux High Assurance Boot (HAB) User's Guide”

from Linux documentation.

https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_LINUXDOCS_BUNDLE&location=null

AN4581

“Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4”

http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf

i.MX Trust Architecture presentation :

https://community.freescale.com/servlet/JiveServlet/download/313957-255581/20-i.MX_TrustArchitecture...

1.

The recent document states, that HAB API may be called from:

- Boot ROM.

− Other boot stages.

−APIs used in U-Boot in this session are:

hab_status_t(*report_event)(hab_status_tstatus, uint32_t index, uint8_t *event, size_t*bytes)

hab_status_t(*report_status)(hab_config_t*config, hab_state_t*state)

2.

Kernel image may be checked by U-boot, as mentioned in “i.MX 6 Linux High Assurance Boot (HAB) User's Guide” :

“The second stage is the authentication of uImage by U-Boot. authenticate_image is called

by U-boot to verify uImage when executing bootm.”

2,666 次查看
satyadamarla
Contributor III

Hello Yuri,

authenticate_image, can this also be done for zImage?

Cheers,

Satya

0 项奖励
回复

2,667 次查看
Yuri
NXP Employee
NXP Employee

Hello,

> authenticate_image, can this also be done for zImage?

Yes.

Regards,

Yuri.

2,666 次查看
Deepu
Contributor III

Hi  Yuri ,

     Thanks a lot for your post .I have all documents except i.MX 6 Linux High Assurance Boot (HAB) User's Guide .This document is very helpfull .Thanks for your help.

0 项奖励
回复