IMX6 platform SDK SD3.0 card support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 platform SDK SD3.0 card support

ソリューションへジャンプ
1,876件の閲覧回数
sergeydanilov
Contributor III

Hello,

Is it possible to work with sd card in UHS-I SDR104 mode (104 MB/s max) using current platform SDK 1.1.0?

in "i.MX 6 Series Firmware Guide" I found the following text (page 348):

For the card initialization process, configure the uSDHC clock as follows:

• Identification frequency ≤ 400 KHz

• Operating frequency ≤ 25 MHz

• High frequency ≤ 50 MHz.


and no any info about SDR104 mode etc.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,309件の閲覧回数
imxcommunitysco
Senior Contributor II

From JackyAtFreescale:

imx6 is compatible with the SDIO Card Specification version 3.0. So it should able to support SDR104.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,310件の閲覧回数
imxcommunitysco
Senior Contributor II

From JackyAtFreescale:

imx6 is compatible with the SDIO Card Specification version 3.0. So it should able to support SDR104.

0 件の賞賛
返信