IMX6 platform SDK SD3.0 card support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 platform SDK SD3.0 card support

跳至解决方案
1,870 次查看
sergeydanilov
Contributor III

Hello,

Is it possible to work with sd card in UHS-I SDR104 mode (104 MB/s max) using current platform SDK 1.1.0?

in "i.MX 6 Series Firmware Guide" I found the following text (page 348):

For the card initialization process, configure the uSDHC clock as follows:

• Identification frequency ≤ 400 KHz

• Operating frequency ≤ 25 MHz

• High frequency ≤ 50 MHz.


and no any info about SDR104 mode etc.

标签 (1)
0 项奖励
回复
1 解答
1,303 次查看
imxcommunitysco
Senior Contributor II

From JackyAtFreescale:

imx6 is compatible with the SDIO Card Specification version 3.0. So it should able to support SDR104.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,304 次查看
imxcommunitysco
Senior Contributor II

From JackyAtFreescale:

imx6 is compatible with the SDIO Card Specification version 3.0. So it should able to support SDR104.

0 项奖励
回复