IMX6 hardware codec support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 hardware codec support

2,567件の閲覧回数
lyfsci
Contributor III

Hi Experts,

What are all the hardware based video/audio codecs which was supported in the IMX6 platforms ?

Regards,

Lyf

ラベル(1)
0 件の賞賛
返信
1 返信

2,138件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

codec specs are provided in Release Notes included in Linux Doc package,

for example in attached L3.14.52 document sect.6.5 Multimedia feature matrix,

which can be obtained from

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信