IMX6 gstreamer pipeline segfault using mfw_mpeg2decoder

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 gstreamer pipeline segfault using mfw_mpeg2decoder

跳至解决方案
9,959 次查看
santox
Contributor II

Hi All,

i'm working with a dvb-t dongle, aiming to watch tv on a MX6Q.

i'm using ltib filesystem with kernel 3.0.35

this is my not-working pipeline:

gst-launch-0.10 dvbbasebin bandwidth=8 code-rate-lp=AUTO code-rate-hp=AUTO guard=AUTO hierarchy=AUTO modulation=AUTO trans-mode=AUTO inversion=AUTO frequency=$f program-numbers=$pn ! mpegtsdemux name=demux ! queue max-size-buffers=0 max-size-time=0 ! mfw_mpeg2decoder ! mfw_v4lsink axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT axis-top=$Y setpara=1

! consider that substituting mfw_mpeg2decoder with ffdec_mpeg2video there is not segfault (but video has frames dropped) !

please give me an hint to solve this problem!

this is my console output:

//-----------------

root@freescale /$ export GST_DEBUG=mfw*:5

MPEG2D_ARM11_02.02.00  build on Apr 19 2011 19:06:38.

MFW_GST_MPEG2_DECODER_PLUGIN 3.0.5 build on Jan 31 2013 08:30:42.

0:00:01.057304156  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:262:mfw_gst_get_first_odev: Get first device:/dev/video16, capabilities 0x4000002

0:00:01.057596823  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[RGBP]RGB565

0:00:01.057674822  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[BGR3]BGR24

0:00:01.057745822  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[RGB3]RGB24

0:00:01.057812822  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[RGB4]RGB32

0:00:01.057879489  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[BGR4]BGR32

0:00:01.057944156  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[NV12]NV12

0:00:01.058009156  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[UYVY]UYVY

0:00:01.058073156  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[YUYV]YUYV

0:00:01.058138489  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[422P]YUV422 planar

0:00:01.058202489  2606    0x17050 WARN             mfw_v4lsink mfw_gst_v4lsink.c:303:mfw_gst_v4l2sink_query_support_formats: unrecognized format:[Y444]YUV444

0:00:01.058268822  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[YU12]YUV420

0:00:01.058333489  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[YV12]YVU420

0:00:01.058397489  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[TNVP]TILED NV12P

0:00:01.058461489  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[TNVF]TILED NV12F

0:00:01.058525155  2606    0x17050 INFO             mfw_v4lsink mfw_gst_v4lsink.c:300:mfw_gst_v4l2sink_query_support_formats: supported format:[444P]YUV444 planar

MFW_GST_V4LSINK_PLUGIN 3.0.5 build on Jan 31 2013 08:29:57.

0:00:01.060863154  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:782:mfw_gst_v4lsink_set_property: axis_top = 0

0:00:01.060979487  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:786:mfw_gst_v4lsink_set_property: axis_left = 0

0:00:01.061081154  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:774:mfw_gst_v4lsink_set_property: width = 800

0:00:01.061181487  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:778:mfw_gst_v4lsink_set_property: height = 450

0:00:01.061282154  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:782:mfw_gst_v4lsink_set_property: axis_top = 85

Setting pipeline to PAUSED ...

0:00:01.062855153  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1468:mfw_gst_v4lsink_change_state:

>>V4LSINK: State: 10

0:00:01.705054828  2606    0x17050 DEBUG            mfw_v4lsink mfw_gst_v4lsink.c:1468:mfw_gst_v4lsink_change_state:

>>V4LSINK: State: 19

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

(gst-launch-0.10:2606): GStreamer-WARNING **: Trying to set string on structure field 'extended-text', but string is not valid UTF-8. Please file a bug.

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

(gst-launch-0.10:2606): GStreamer-WARNING **: Trying to set string on structure field 'extended-text', but string is not valid UTF-8. Please file a bug.

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

(gst-launch-0.10:2606): GStreamer-WARNING **: Trying to set string on structure field 'extended-text', but string is not valid UTF-8. Please file a bug.

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

(gst-launch-0.10:2606): GStreamer-WARNING **: Trying to set string on structure field 'extended-text', but string is not valid UTF-8. Please file a bug.

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso8859-9' to 'utf-8' is not supported

(gst-launch-0.10:2606): GStreamer-WARNING **: Trying to set string on structure field 'extended-text', but string is not valid UTF-8. Please file a bug.

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

** (gst-launch-0.10:2606): CRITICAL **: Could not convert string: Conversion from character set 'iso6937' to 'utf-8' is not supported

0:00:08.375314161  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1007:mfw_gst_mpeg2dec_sink_event: handling newsegment event

0:00:08.375504494  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1019:mfw_gst_mpeg2dec_sink_event:  receiving new seg

0:00:08.375590828  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1020:mfw_gst_mpeg2dec_sink_event:  start = 20:22:25.317944444

0:00:08.375658161  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1021:mfw_gst_mpeg2dec_sink_event:  stop = 99:99:99.999999999

0:00:08.375721828  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1024:mfw_gst_mpeg2dec_sink_event:  position in mpeg2dec   =0:00:00.000000000

0:00:08.375952161  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1116:mfw_gst_mpeg2dec_set_caps:  in mfw_gst_mpeg2dec_set_caps function

0:00:08.376037828  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:1127:mfw_gst_mpeg2dec_set_caps:  Frame Rate = nan

0:00:08.376215828  2606   0x106348 DEBUG       mfw_mpeg2decoder mfw_gst_mpeg2dec.c:681:mfw_gst_mpeg2dec_chain:

Coming for the first time to do the decoder                          initialization

Caught SIGSEGV accessing address 0x14

Spinning.  Please run 'gdb gst-launch 2606' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.

root@freescale /$

//-----------------

标签 (6)
1 解答
7,557 次查看
karina_valencia
NXP Apps Support
NXP Apps Support
Re: IMX6 gstreamer pipeline segfault using mfw_mpeg2decoder

Jian LiEmployee

customer is using mpegtsdemux, which is listed in gst-plugins-bad package, not sure if this plugin can work correctly with the ts stream. One way customer can try is to play the ts file from local disk with this plugin to see if still have the AV out of sync issue, if yes, it's this plugins issue.

There are some other open source plugins for ts demux, customer also can have a try: tsdemux, tsparse, mpegtsparse.

在原帖中查看解决方案

0 项奖励
回复
22 回复数
7,061 次查看
santox
Contributor II

Finally i solved my smoothness troubles upgrading gst-plugins-bad to version 0.10.22 and using "tsdemux" demuxer.

Thank you all for your support.

But i'm not out of issues : when i tune on some channels i have this warning on console:

GStreamer-WARNING **: Trying to set string on structure field'description', but string is not valid UTF-8. Please file a bug

do someone knows what i'm missing?

i installed libiconv in ltib; but i noticed i miss /usr/lib/gconv folder; maybe this is my problem? how to have  /usr/lib/gconv folder correctly installed?

0 项奖励
回复
7,061 次查看
morenohassem
Contributor I

I know you probably solved your problem, but to me it looks like you have a clock problem. Have you tried sync=no on the v4lsink?

Regards!

0 项奖励
回复
7,061 次查看
santox
Contributor II

As explained upper in this discussion,

i'm using mpegtsdemux (the one in gst-plugins-bad bundled in ltib 4.0.0).

Playing from local disk (you can download stream.ts from DepositFiles) , instead of streaming live, i experience the same framedrop issue that, using  IMX6's vpudec, entail the audio/video out-of-sync (~10sec/60sec of video are dropped!!!, after ~1min audio is ~10 sec later than video... actually video is ahead than audio)  . On PC, using mpeg2dec, the local stream.ts  is played smoothly, with in-sync audio.

The gst-plugins-bad version bundled in ltib misses tsdemux plugin. I'll upgrade the package to a newer version and give a try to tsdemux.

0 项奖励
回复
7,062 次查看
santox
Contributor II

ok, switched to LTIB 4.0.0, nothing changed.

also, this message remains:

[WARN] VPU iram is less than needed, some parts don't use iram

i have a video captured **from my PC** with the following commandline:

cat /dev/dvb/adapter0/dvr0 > /tmp/stream.ts #ctrl+C after ~60sec

its reproduced smoothly (audio and video in sync!) on the PC with following pipeline

pn=8585

cat /tmp/stream.ts | gst-launch-0.10 fdsrc fd=0 ! mpegtsdemux program-number=$pn name=demux ! queue max-size-buffers=0 max-size-time=0 ! mpeg2dec ! xvimagesink demux. ! queue max-size-buffers=0 max-size-time=0 ! mad ! alsasink

fyi these are the programs contained into the stream:

Rai Premium:514000000:INVERSION_AUTO:BANDWIDTH_8_MHZ:FEC_2_3:FEC_AUTO:QAM_64:TRANSMISSION_MODE_8K:GUARD_INTERVAL_1_32:HIERARCHY_NONE:431:441:8581

Rai yoyo:514000000:INVERSION_AUTO:BANDWIDTH_8_MHZ:FEC_2_3:FEC_AUTO:QAM_64:TRANSMISSION_MODE_8K:GUARD_INTERVAL_1_32:HIERARCHY_NONE:432:442:8582

Rai 4:514000000:INVERSION_AUTO:BANDWIDTH_8_MHZ:FEC_2_3:FEC_AUTO:QAM_64:TRANSMISSION_MODE_8K:GUARD_INTERVAL_1_32:HIERARCHY_NONE:433:443:8583

Rai Gulp:514000000:INVERSION_AUTO:BANDWIDTH_8_MHZ:FEC_2_3:FEC_AUTO:QAM_64:TRANSMISSION_MODE_8K:GUARD_INTERVAL_1_32:HIERARCHY_NONE:434:445:8584

Rai Movie:514000000:INVERSION_AUTO:BANDWIDTH_8_MHZ:FEC_2_3:FEC_AUTO:QAM_64:TRANSMISSION_MODE_8K:GUARD_INTERVAL_1_32:HIERARCHY_NONE:435:446:8585

on target i.MX6 DualLite i use following pipeline:

pn=8585

export WIDTH=800

export HEIGHT=450

export Y=85

cat stream.ts | gst-launch-0.10 fdsrc fd=0 ! \

mpegtsdemux program-number=$pn name=demux ! queue max-size-buffers=0 max-size-time=0 ! vpudec ! mfw_v4lsink axis-top=0 axis-left=0 disp-width=$WIDTH disp-height=$HEIGHT axis-top=$Y setpara=1 \

demux. ! queue max-size-buffers=0 max-size-time=0 ! mad ! alsasink &

audio is out of sync (seconds late..), it seems this happens because some frames are dropped (on the "real case" where the source is live and not recorded on disk, video is also stuttering.)

this is cpu load:

  PID PPID USER STAT VSZ %VSZ CPU %CPU COMMAND

3008 2708 root S 78100 12.2 0 6.4 gst-launch-0.10 fdsrc fd=0 ! mpegt

p.s.: wher can i upload the file stream.ts so you can try to reproduce the issue? it is ~150MB

7,062 次查看
santox
Contributor II

you can download stream.ts here:

http://dfiles.eu/files/qps2mhpon

0 项奖励
回复
7,558 次查看
karina_valencia
NXP Apps Support
NXP Apps Support
Re: IMX6 gstreamer pipeline segfault using mfw_mpeg2decoder

Jian LiEmployee

customer is using mpegtsdemux, which is listed in gst-plugins-bad package, not sure if this plugin can work correctly with the ts stream. One way customer can try is to play the ts file from local disk with this plugin to see if still have the AV out of sync issue, if yes, it's this plugins issue.

There are some other open source plugins for ts demux, customer also can have a try: tsdemux, tsparse, mpegtsparse.

0 项奖励
回复
7,062 次查看
santox
Contributor II

i noticed this message in gstreamer output:

[WARN]  VPU iram is less than needed, some parts don't use iram

what's that mean?

i also notice jerky video output, audio/video out-of-sync and sometimes i lost audio.... some hints?

0 项奖励
回复
7,062 次查看
daiane_angolini
NXP Employee
NXP Employee

about audio/video out of sync, are you sure your media file is in sink? Have you tried to play it on your PC using, like, VLC?

About the gstreamer output, I´m not sure, maybe karinavalencia could point someone to help on this.

What do you mean by jerky? Have you tried to drop some frames?

0 项奖励
回复
7,062 次查看
santox
Contributor II

my source is a dvb-t tv dongle. No problems with similar pipeline on my pc; no problems with mplayer and vlc too on pc.

i suspect vpudec is losing frames... i experience "occasional" stuttering (it's smooth for a couple of secs, but then some stutter... and after it's smooth for some other sec... etc... and the audio gets out of sync.)

Sometimes the pipeline "starts badly" and i experience really bad audio jittering

any option to obtain better results? buffering? some kernel optimization? some fancy option in the gstreamer pipeline elements?

0 项奖励
回复
7,061 次查看
LeonardoSandova
Specialist I

There is a framedrop parameter on vpudec, set it false and see if that helps. Also post your question to the gstreamer-devel list, and ask if your pipeline can be tuned a for better performance. A suggestion: In order to identify the video artifacts you are seeing, do not add the audio elements into the pipeline.

Leo

7,062 次查看
santox
Contributor II

setting vpudec framedrop=false results in really bad stuttering after a few secs, after a (really small) while image freezes and gets updated only every few sec

0 项奖励
回复
7,062 次查看
LeonardoSandova
Specialist I

I see. In the other hand, This is a time to create your own packages on your current BSP, so moving to 4.0.0 is not so hard :smileyhappy: Not sure if you will see any improvement on that particular pipeline but it is worth trying it 4.0.0. it has all fixes and improvements on all layers, including GST.

Leo

7,062 次查看
daiane_angolini
NXP Employee
NXP Employee

Thanks for your reply.

No, I don´t know any other fancy option for gstreamer. No one that you would not know, at least. (queues, caps, this stuff)

Did you tried using the latest plugins from 4.0.0 BSP?

0 项奖励
回复
7,062 次查看
santox
Contributor II

uhm, no, did not noticed a new BSP release! I'm with the previous one.... downloading 4.0.0... i'm not really excited to install it from scratch and apply all my modifications and packages on it.. :smileysad:

is it present an "update" feature i'm not aware of?

thank you all for support and good suggestions.

0 项奖励
回复
7,062 次查看
daiane_angolini
NXP Employee
NXP Employee

Please give 4.0.0 a try, or only take a look in the release notes. If you think it's not enough, please, reopen this thread (it's marked as "answered", please, unmark that)

And try to get a way we can reproduce the issue you see. I don't have an dvb-t dongle but you may create a movie to reproduce the same behavior. This way we can reproduce and even escalate the issue.

0 项奖励
回复
7,062 次查看
santox
Contributor II

i'm able to play movies using gplay and also using playbin2; but in this case it's not a movie, it's a live streaming from a dvb-t dongle source... so i need to write my pipeline; i'm trying to get best performance possible using hw acceleration whereever possible.

0 项奖励
回复
7,062 次查看
daiane_angolini
NXP Employee
NXP Employee

Oh, sorry.

demux

the demux provided by freescale is not hardware accelerated. It has some "optimization" for the hardware, but it is not developed for streaming packages, it was tested using media files. I mean, I´m not sure it would be your best choice. You should consider to calculate the performance for both cases and decide which one is the best (i mean, compare freescale with opensource plugin)

video decoder

Was you able to decode it?

audio decoder

When you try a local media file, does beepdec work?

0 项奖励
回复
7,062 次查看
santox
Contributor II

Hi Daiane, thank you for your reply.

currently my best result is using the following pipeline:

     dvbbasebin !  mpegtsdemux

          ! vpu_dec ! mfw_v4lsink !

          ! mad ! alsasink

demux: using aiurdemux my pipeline doesn't start rolling... remains "freezed" waiting for can't say what. is still the issue described in https://community.freescale.com/thread/269124 present?

video decoder: yes i had success using either mpeg2dec, ffdec_mpeg2video or vpudec

audio decoder: i had troubles also trying to play a local mp3 using beepdec; mad worked fine.

0 项奖励
回复
7,062 次查看
daiane_angolini
NXP Employee
NXP Employee

luca santini wrote:

Hi Daiane, thank you for your reply.

currently my best result is using the following pipeline:

     dvbbasebin !  mpegtsdemux

          ! vpu_dec ! mfw_v4lsink !

          ! mad ! alsasink

demux: using aiurdemux my pipeline doesn't start rolling... remains "freezed" waiting for can't say what. is still the issue described in https://community.freescale.com/thread/269124 present?

I don´t know, you and the link are using completely different gst-plugins versions. As I know aiurdemux is not optimized to streaming (over ethernet or something like that). As you have your mpegtsdemux I would keep it.

video decoder: yes i had success using either mpeg2dec, ffdec_mpeg2video or vpudec

audio decoder: i had troubles also trying to play a local mp3 using beepdec; mad worked fine.

My local tests (not official and not properly verified) shows that beepdec and mad has almost the same cpu load. I would keep using mad.

What´s your status right now? (I mean, I think I missed the goal here)

0 项奖励
回复
7,062 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

no more comments  from customer.

0 项奖励
回复