IMX6 boot problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 boot problem

1,971件の閲覧回数
srinivasaporam
Contributor II

Hi,

we have got customized board based on IMX6 Dual processor. Now when we have deployed linux image to the SD card and powering on the board, then nothing is happening ( no display is shown) ( monitor is connected to board through HDMI)

When we keep the same sd card to another evaluation board, then it is booting. Now to trace out the problem:

how i can confirm the processor trying to read/boot from the sd card, which happening but there is problem with the HDMI.

or

SD card reading is not happening.

how trace down where the problem is . when i connect the board to my Ubuntu host system through USB-OTG and run the command $lsusb

iam getting following message:

Bus 001 Device 006: ID 0bda:58c2 Realtek Semiconductor Corp.

Bus 001 Device 005: ID 0bda:0129 Realtek Semiconductor Corp. RTS5129 Card Reader Controller

Bus 001 Device 007: ID 0cf3:0036 Atheros Communications, Inc.

Bus 001 Device 003: ID 046d:c077 Logitech, Inc.

Bus 001 Device 014: ID 15a2:0054 Freescale Semiconductor, Inc. i.MX6Q SystemOnChip in RecoveryMode

Bus 001 Device 002: ID 8087:8000 Intel Corp.

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

Bus 003 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub

Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

and one more query, our board has got: MCIMX6D5EYM10AC, but why is it getting detected as:

Freescale Semiconductor, Inc. i.MX6Q SystemOnChip in RecoveryMode

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,814件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Srinivasa

seems board falls to serial serial downloader,

in this mode in host computer device manager one

could see usb device:

MX6D vid="15A2" pid="0061"

MX6Q vid="15A2" pid="0054"

It may be recommended to check boot settings and Chapter 8

Avoiding Board Bring-up Problems IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,814件の閲覧回数
srinivasaporam
Contributor II

Hi,

Our board has got MCIMX6D5EYM10AC chip which should be dual core since it has 6D not 6Q. But when we are connecting the board to host (Ubuntu) system and running lsusb command , then output is :

Bus 001 Device 006: ID 0bda:58c2 Realtek Semiconductor Corp.

Bus 001 Device 005: ID 0bda:0129 Realtek Semiconductor Corp. RTS5129 Card Reader Controller

Bus 001 Device 007: ID 0cf3:0036 Atheros Communications, Inc.

Bus 001 Device 003: ID 046d:c077 Logitech, Inc.

Bus 001 Device 014: ID 15a2:0054 Freescale Semiconductor, Inc. i.MX6Q SystemOnChip in RecoveryMode

Bus 001 Device 002: ID 8087:8000 Intel Corp.

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

Bus 003 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub

Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

If we see the output carefully it is detected as "Bus 001 Device 014: ID 15a2:0054 Freescale Semiconductor, Inc. i.MX6Q SystemOnChip in RecoveryMode" which Quad. is this normal??? any problem???? how to get confirmed which is correct one???

0 件の賞賛
返信