IMX6 android5.0.2 user load cannot boot up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 android5.0.2 user load cannot boot up

1,728 Views
bincao
Contributor I

Hello,

IMX6 android5.0.2 user load cannot boot up,relative log as below,

01-01 00:02:01.879 F/dex2oat (  429): art/runtime/runtime.cc:284]

01-01 00:02:01.879 F/libc    (  429): Fatal signal 6 (SIGABRT), code -6 in tid 429 (main)

01-01 00:02:01.981 I/DEBUG   (  152): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

01-01 00:02:01.981 I/DEBUG   (  152): Build fingerprint: 'Freescale/em70/em70:5.0.2/1.0.0-ga-rc4/10200211:user/release-keys'

01-01 00:02:01.981 I/DEBUG   (  152): Revision: '0'

01-01 00:02:01.981 I/DEBUG   (  152): ABI: 'arm'

01-01 00:02:01.981 I/DEBUG   (  152): pid: 429, tid: 429, name: main  >>> /system/bin/dex2oat <<<

01-01 00:02:01.981 I/DEBUG   (  152): signal 6 (SIGABRT), code -6 (SI_TKILL), fault addr --------

01-01 00:02:02.010 I/DEBUG   (  152): Abort message: 'art/runtime/runtime.cc:820] Check failed: options->boot_class_path_ != nullptr '

01-01 00:02:02.010 I/DEBUG   (  152):     r0 00000000  r1 000001ad  r2 00000006  r3 00000000

01-01 00:02:02.010 I/DEBUG   (  152):     r4 76f8b114  r5 00000006  r6 00000002  r7 0000010c

01-01 00:02:02.010 I/DEBUG   (  152):     r8 00000001  r9 7664f490  sl 76607400  fp 766501c0

01-01 00:02:02.010 I/DEBUG   (  152):     ip 000001ad  sp 7e88bf60  lr 76f14119  pc 76f38344  cpsr 600f0010

01-01 00:02:02.010 I/DEBUG   (  152):

01-01 00:02:02.010 I/DEBUG   (  152): backtrace:

01-01 00:02:02.010 I/DEBUG   (  152):     #00 pc 0003b344  /system/lib/libc.so (tgkill+12)

01-01 00:02:02.010 I/DEBUG   (  152):     #01 pc 00017115  /system/lib/libc.so (pthread_kill+52)

01-01 00:02:02.010 I/DEBUG   (  152):     #02 pc 00017d33  /system/lib/libc.so (raise+10)

01-01 00:02:02.011 I/DEBUG   (  152):     #03 pc 00014589  /system/lib/libc.so (__libc_android_abort+36)

01-01 00:02:02.011 I/DEBUG   (  152):     #04 pc 00012a40  /system/lib/libc.so (abort+4)

01-01 00:02:02.011 I/DEBUG   (  152):     #05 pc 00215895  /system/lib/libart.so (art::Runtime::Abort()+160)

01-01 00:02:02.011 I/DEBUG   (  152):     #06 pc 000a6e93  /system/lib/libart.so (art::LogMessage::~LogMessage()+1322)

01-01 00:02:02.011 I/DEBUG   (  152):     #07 pc 00217c4d  /system/lib/libart.so

(art::Runtime::Init(std::__1::vector<std::__1::pair<std::__1::basic_string<char, std::__1::char_traits<char>, std::__1::allocator<char> >, void const*>, std::__1::allocator<std::__1::pair<std::__1::basic_string<char, std::__1::char_traits<char>, std::__1::allocator<char> >, void const*> > > const&, bool)+4944)

01-01 00:02:02.011 I/DEBUG   (  152):     #08 pc 0021880b  /system/lib/libart.so (art::Runtime::Create(std::__1::vector<std::__1::pair<std::__1::basic_string<char, std::__1::char_traits<char>, std::__1::allocator<char> >, void const*>, std::__1::allocator<std::__1::pair<std::__1::basic_string<char, std::__1::char_traits<char>, std::__1::allocator<char> >, void const*> > > const&, bool)+46)

01-01 00:02:02.011 I/DEBUG   (  152):     #09 pc 0000aa09  /system/bin/dex2oat

01-01 00:02:02.011 I/DEBUG   (  152):     #10 pc 0000deaf  /system/bin/dex2oat

01-01 00:02:02.011 I/DEBUG   (  152):     #11 pc 000128f1  /system/lib/libc.so (__libc_init+44)

01-01 00:02:02.011 I/DEBUG   (  152):     #12 pc 00006508  /system/bin/dex2oat

01-01 00:02:02.072 I/DEBUG   (  152):

01-01 00:02:02.072 I/DEBUG   (  152): Tombstone written to: /data/tombstones/tombstone_01

01-01 00:02:02.073 E/installd(  155): DexInv: --- END '/system/framework/services.jar' --- status=0x0006, process failed

01-01 00:02:02.074 I/art     (  416): DexFile_isDexOptNeeded failed to open oat file '/data/dalvik-cache/arm/system@[email protected]@classes.dex' for file location '/system/framework/ethernet-service.jar': Failed to open oat filename for reading: No such file or directory

01-01 00:02:02.074 I/art     (  416): DexFile_isDexOptNeeded failed to open oat file '/system/framework/arm/ethernet-service.odex' for file location '/system/framework/ethernet-service.jar': Failed to open oat filename for reading: No such file or directory

01-01 00:02:02.108 E/cutils-trace(  431): Error opening trace file: Permission denied (13)

what's the root cause of this crash issue? I see no odex files generated under system folder, but other 5.0 deivces like nexus have odex files generated, so is this the possible

reason. Besides, I found there is a code change in dex_preopt_libart.mk, LIBART_IMG_TARGET_BASE_ADDRESS := 0x50000000, what does this change mean? Could you

give me a suggest to fix this issue and boot up successfully?

Thanks!

0 Kudos
Reply
1 Reply

1,291 Views
bincao
Contributor I

Hi All,

Anybody had found the same issue and give me a suggestion? Should set WITH_DEXPREOPT true, but seems having build error?

0 Kudos
Reply