IMX6:USB not able to enumerate UVC device (webcam)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6:USB not able to enumerate UVC device (webcam)

跳至解决方案
8,082 次查看
anjojohn
Contributor IV

Hi All,

We have USB webcam connected to imx6 custom board. IMX6 is not able to enumerate the device. shows below print

[ 151.603744] usb 1-1: new high-speed USB device number 70 using ci_hdrc
[ 152.812637] usb 1-1: unable to read config index 0 descriptor/start: -71
[ 152.818633] usb 1-1: can't read configurations, error -71

If i connect the same camera to PC , it gets detected and UVC device is enumerated. 

further more if a connect a USB HUB between the imx6 board and camera , the camera is detected and there is no problem taking the video stream.

 USB camera is only able to get enumerated with a HUB connected in between. Is this due to any error in USB device descriptor query commands. I have tried with latest kernel 4.1.2 . it also have same issue.  Also tested other USB devices  keyboard,mouse, pen-drive all are getting enumerated without a HUB.

Any help is appreciated.

Thanks

标签 (4)
1 解答
7,415 次查看
igorpadykov
NXP Employee
NXP Employee

Hi anjo

connecting through hub usually used for finding source of usb misbehaviour with

data integrity or poor signals are suspected. One can try to tweak usb signal

with procedures described in AN4589 Configuring USB on i.MX 6 Series Processors

https://www.nxp.com/docs/en/application-note/AN4589.pdf 

Another reason may be that power provided to web camera from i.MX side is insufficient.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
6,027 次查看
nadimfnadaf
Contributor III

Hi  @all

dmesg output is :

usb 1-1: unable to get BOS descriptor set
usb 1-1: unable to read config index 0 descriptor/all
usb 1-1: can't read configurations, error -71
usb 1-1: new high-speed USB device number 7 using ci_hdrc
usb 1-1: unable to get BOS descriptor set
usb 1-1: unable to read config index 0 descriptor/all
usb 1-1: can't read configurations, error -71
usb 1-1: new high-speed USB device number 8 using ci_hdrc
usb 1-1: device not accepting address 8, error -71
usb 1-1: new high-speed USB device number 9 using ci_hdrc
usb 1-1: device not accepting address 9, error -71
usb usb1-port1: unable to enumerate USB device

But this solution doesn't work in my case. 

Any help is appreciated.

Thanks

标记 (1)
0 项奖励
回复
7,415 次查看
alcotross02
Contributor I

Hello Anjo! I'm trying to get my USB webcam to work. I think I have the right stuff in the kernel built-in (or as modules) but when I plug it in I get funny errors: 

USB port 2: [  444.165188] usb 8-2: Not enough bandwidth for altsetting 11 
[ 2853.264080] usb 8-2: USB disconnect, device number 3 
[ 2857.410263] usb 3-4: new high-speed USB device number 2 using ehci_hcd 
[ 2857.529914] usb 3-4: device descriptor read/64, error -32 
[ 2857.759256] usb 3-4: device descriptor read/64, error -32 
[ 2857.988597] usb 3-4: new high-speed USB device number 3 using ehci_hcd 
[ 2858.108254] usb 3-4: device descriptor read/64, error -32 
[ 2858.337597] usb 3-4: device descriptor read/64, error -32 
[ 2858.566937] usb 3-4: new high-speed USB device number 4 using ehci_hcd 

USB Port 3:  [ 3278.175163] usb 8-2: Not enough bandwidth for altsetting 1 
[ 3278.175164] 12:3:1: usb_set_interface failed (-22) 
[ 3278.175369] xhci_hcd 0000:02:00.0: ERROR: unexpected command completion code 0x11. 
[ 3278.175372] usb 8-2: Not enough bandwidth for altsetting 1 
[ 3278.175373] 12:3:1: usb_set_interface failed (-22)

If any problem with the Netgear Arlo security camera, then you can try on netgear arlo support, I hope that all the information you can gets from here.

Have a Good Day!!!

0 项奖励
回复
7,416 次查看
igorpadykov
NXP Employee
NXP Employee

Hi anjo

connecting through hub usually used for finding source of usb misbehaviour with

data integrity or poor signals are suspected. One can try to tweak usb signal

with procedures described in AN4589 Configuring USB on i.MX 6 Series Processors

https://www.nxp.com/docs/en/application-note/AN4589.pdf 

Another reason may be that power provided to web camera from i.MX side is insufficient.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

7,415 次查看
anjojohn
Contributor IV

Hi Igor,

Thank you for the response. Issue has been fixed. It was due to lengthy USB OTG cable. After using short OTG cable camera got enumerated.

0 项奖励
回复