IMX6 Solo Reference Design.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Solo Reference Design.

2,616 Views
sanjayshekar
Contributor I

Hello Freescale,

        We are looking to use Imx6 solo as our solution for one of our customer product.

Below are few queries I have.

1. Do we have any reference design for Imx6 Solo in specific??

2. Imx6 Solo and Imx6 solo lite are pin compatible ??

3. Can we use Imx6LELK as the reference design and replace  Solo lite with Solo SOC or any other suggestion?? (of course with some required changes.)

4. How would we check if the BSP supports the required Codecs?? Like for example for kitkat BSP available from freescale, if we need "xyz" codec, if kitkat supports it and also the processor does, can we say that the BSP available from freescale has this codec support??  

your support is appreciated and will help us is proceeding further for a decision :smileyhappy:

Regards,

Sanju.

Labels (3)
0 Kudos
Reply
1 Reply

1,566 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

1. Do we have any reference design for Imx6 Solo in specific??

Have a look at the SDP board

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT

You have the MX6DL/S dedicated board : MCIMX6DL-SDP

2. Imx6 Solo and Imx6 solo lite are pin compatible ??

No, Solo/Dual Lite/Dual/Quad are.

3. Can we use Imx6LELK as the reference design and replace Solo lite with Solo SOC or any other suggestion?? (of course with some required changes.)

No, use MCIMX6DL-SDP

4. How would we check if the BSP supports the required Codecs?? Like for example for kitkat BSP available from freescale, if we need "xyz" codec, if kitkat supports it and also the processor does, can we say that the BSP available from freescale has this codec support??

Check Android BSP documentation, user guide and release notes, etc.

http://www.freescale.com/webapp/Download?colCode=IMX6_KK443_200_ANDROID_DOCS&Parent_nodeId=133769948...

Best Regards,

Luis

0 Kudos
Reply