Hello,
I have built uImage using Genode OS Framework for IMX6 Sabre SDBoard. I am using u-Boot built for iMX6 Board. I am getting error as cannot get kernel image.
My built uImage is 7858662 Bytes = 7.5 MB
I used following commands to flash u-boot and uImage respectively (It is a 16GB microsdcard)
$sudo dd if=u-Boot-mx6q-sabresd-no-padding.bin of=/dev/sdc bs=512 seek=2 conv=fsync
$sudo dd if=uImage of=/dev/* bs=512 seek=2048 conv=fsync
When I inserted the SDCard to the board and tried to boot, it is giving the following error:
## Booting kernel from Legacy Image at 10800000 ...
Image Name:
Image Type: ARM Linux Kernel Image (gzip compressed)
Data Size: 7858662 Bytes = 7.5 MB
Load Address: 10001000
Entry Point: 10001000
Verifying Checksum ... Bad Data CRC
ERROR: can't get kernel image!
Kindly Suggest.