IMX6 SDMA ROM Script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 SDMA ROM Script

Jump to solution
2,864 Views
ahmedabdelhalee
Contributor II

Dear All,

Where can I find the source code of the IMX6Q SDMA ROM script [that channel 0 executes during booting]?

I can found the source code for IMX51 on : (git://git.pengutronix.de/git/imx/sdma-firmware.git) but couldn't find the equivalent for IMX6Q.

Please reply ASAP.

Thanks in advance,

Ahmed

Labels (1)
0 Kudos
Reply
1 Solution
2,198 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ahmed

usually Freescale does not disclose rom sources, however

you can try entering SR ticket. Also you should provide solid reasons

why they are necessary for you.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,199 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ahmed

usually Freescale does not disclose rom sources, however

you can try entering SR ticket. Also you should provide solid reasons

why they are necessary for you.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply